SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Unregisters an interrupt handler for a I2S interrupt.
Parameters:
ulBasethe base address of the I2S moduleThis function unregisters the interrupt handler. The function clears the handler to be called when an I2S interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
See
IntRegister()
for information about registering interrupt handlers.
Returns:
None