SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
MCU Reset (Software Reset)
The MCU subsystem can be reset to its default state using the following API function call.
void PRCMMCUReset(tBoolean bIncludeSubsystem)
Description: This function performs a software reset of the MCU and associated peripherals. The core resumes execution in the ROM bootloader, which reloads the user application from sFlash.
Parameter: bIncludeSubsystem – If true, the MCU and its associated peripherals are reset; if false, only the MCU is reset.
Return: None