The content from one of the two analog banks can be read out by:
- Driving the SEN pin low.
- Selecting the page address of the register whose content must be read.
- Master page: write address 0011h with 80h.
- ADC page: write address 0011h with 0Fh.
- Setting the R/W bit to 1 and writing the address to be read back.
- Reading back the register content on the SDOUT pin, as shown in Figure 8-14. When a page is selected, multiple read backs from the same page can be done. SDOUT comes out at the SCLK falling edge with an approximate delay (tSD_DELAY) of 68 ns; see Figure 8-18.