ZHCSEA4C May 2015 – December 2020 ADS54J40
PRODUCTION DATA
The fast OVR is triggered if the input voltage exceeds the programmable overrange threshold and is presented after only 18 clock cycles + tPD (tPD of the gates and buffers is approximately 4 ns), thus enabling a quicker reaction to an overrange event.
The input voltage level that the overload is detected at is referred to as the threshold. The threshold is programmable using the FOVR THRESHOLD bits, as shown in Figure 8-11. The FOVR is triggered 18 clock cycles + tPD (tPD of the gates and buffers is approximately 4 ns) after the overload condition occurs.
Figure 8-11 Programming Fast OVR ThresholdsThe input voltage level that the fast OVR is triggered at is defined by Equation 2:
The default threshold is E3h (227d), corresponding to a threshold of –1 dBFS.
In terms of full-scale input, the fast OVR threshold can be calculated as Equation 3: