SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
Every IP working on SYS_CLK has a separate clock gate. In the case that clock gate is implemented in the IP, clock is routed directly to the IP with no clock gate inserted at the SOC-level. The diagram below shows the generic structure for all IP sourced from SYS_CLK.
Figure 6-25 Generic IP clocking with
SYS_CLKIn the case that the peripherals implement clock gating internal to the IP, no additional ICG is provisioned in RCM.