SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The SoC has many peripherals and a large number of event sources including interrupts, time sync events, and DMA requests. The use of events is completely dependent on a user's specific application, which drives a need for maximum flexibility on which event sources are used in the system. Software control must be used to service these events.
The SoC includes the following interrupt servicing modules (hosts):
Most of the system events are routed directly to the various processing elements but in some cases it is impractical to route all events of a certain group (for example, GPIO events) to each processing element. For this purpose, the SoC integrates several interrupt router (INTRTR) instances. Each interrupt router aggregates a number of system events and can route each event to a given processing element by using simple combinational logic (implemented via a set of multiplexors). Event selection is controlled through the associated registers within each interrupt router.
The following interrupt router instances are part of the SoC interrupt architecture:
In addition, the following interrupt router instances are part of the SoC time sync architecture: