SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The extended Message ID (29-bit ID) filtering flow is shown in Figure 13-214. Section 13.4.1.4.10.6, Extended Message ID Filter Element describes the extended Message ID filter element.
The Remote Transmission Request (RTR) and Extended Identifier (XTD) bits of the received frames are compared against the list of configured filter elements. This is controlled by the following registers:
Note that before the filter list is executed the received identifier is ANDed with the Extended ID AND Mask (MCAN_XIDAM).
Figure 13-215 Extended Message ID Filter Path