SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
Error Interrupt Outputs are provided so that a processor in the SoC can be signaled to intervene when an Error Event occurs. Each error event input can be enabled, via software, to cause an Error Interrupt to occur (Error Group N Interrupt Enabled Set Register (Base Address + 0x400 + N*0x20 + 0x08)). Additionally, each error event input can be programmed to influence either the Low Priority (Default) interrupt or the High Priority interrupt (Error Group N Interrupt Priority Register (Base Address + 0x400 + N*0x20 + 0x10)). The Low Priority interrupt is intended for events that are of interest, but do not require immediate intervention. For example, an indication that there was a single bit error that was corrected may signal a low priority interrupt, so that information can be collected for statistical purposes. A High Priority interrupt is intended for events that need immediate attention. For example, an indication that there was an uncorrected two-bit error may be signaled as a high priority interrupt.