SLUUCH2 March 2021 BQ40Z50-R2
By default, if there is an RSOC of 20.1 through 20.9, then the RSOC becomes 21 (ceiling function). However, the following shows how the RSOC rounding feature works when enabled by setting [RSOC_RND_OFF] = 1 (default is 0) in the SBS Gauging Configuration register:
Round-off applies to charging and discharging between an RSOC 0% to 99% if, for example:
There is an RSOC of 20.1 through 20.4, then the RSOC becomes 20 (round off).
There is an RSOC of 20.5 through 20.9, then the RSOC becomes 21 (round off).
Round-down applies for charging and discharging between an RSOC of 99% to 99.9% if:
There is an RSOC of 99.1 or 99.9, then the RSOC becomes 99 (round down).
In charge, RSOC is set to 100% only when FC is set.