ZHCSN24A August 2019 – May 2021 TPS53676
PRODUCTION DATA
The nominal on-time for each phase is determined by an adaptive one-shot circuit, which generates on-times according to Equation 34. PWM on-times are adjusted very slowly compared to off-times, so the DCAP+ modulator behaves similar to a constant-on-time architecture.
Use the FREQUENCY_SWITCH command to set the nominal per-phase switching frequency.
where
Current sharing is implemented by adapting the on-time for each phase, according to the difference between its own phase current IL, and the average of all phase currents IAVG. When the phase current for any one phase is greater than the average of all phase currents, the on-time of that phase is reduced accordingly. Similarly, if the phase current of any one phase is less than the average of all phase currents, the on-time of that phase is increased.
The on-time is also proportional to the sensed input voltage, which provides the controller with inherent input voltage feed-forward.
Furthermore, a frequency control loop adjusts the on-times for each phase to drive the actual switching frequency equal to the FREQUENCY_SWITCH setting. An internal clock counts the number of observed pulses over a set interval, and compares the result to the calculated ideal number. If too many pulses are fired in the sampling period, the switching frequency is too high, and the on-times are increased to reduce the steady-state switching frequency. If too few pulses are fired during the sampling period, the switching frequency is too low and the on-times are reduced to increase the steady-state frequency. The PWM pin assigned to ORDER=0 is used for counting purposes, as it does not drop due to phase shedding.
Figure 7-22 On-time generation and auto-balance current sharing