SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The transfer signal sequence for Freescale SPI format with SPO=1 and SPH=1 is shown in Figure 47-9, which covers both single and continuous transfers.
Figure 47-9 Freescale SPI Frame Format
with SPO =1 and SPH =1
In this configuration, during idle periods:
If the SSI is enabled and valid data is in the transmit FIFO, the start of transmission is signified by the SSIFss master signal being driven low. The master SSITx output pad is enabled. After an additional one-half SSIClk period, both master and slave data are enabled onto their respective transmission lines. At the same time, SSIClk is enabled with a falling edge transition. Data is then captured on the rising edges and propagated on the falling edges of the SSIClk signal.
After all bits have been transferred, in the case of a single word transmission, the SSIFss line is returned to its idle high state one SSIClk period after the last bit has been captured.
For continuous back-to-back transmissions, the SSIFss pin remains in its active low state until the final bit of the last word has been captured and then returns to its idle state as described above.
For continuous back-to-back transfers, the SSIFss pin is held low between successive data words and termination is the same as that of the single word transfer.