SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The High Level Controller (HLC) is significantly more complex than the other blocks in the CLB tile. The HLC performs two main functions:
The architecture of the HLC is shown in Figure 9-20. The HLC is an event-based system capable of handling up to four simultaneous events that can be selected from any outputs of the other blocks within the tile or from an external input.
Figure 9-20 High Level Controller
Block