SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The timestamp maintained in the MAC is 64-bit wide. The overflow to upper 16-bits of seconds register happens once in 130 years. The values of the upper 16-bits of the seconds field can be read from the CSR register.
This is provided to use an additional Higher Word Register.
This higher word register can be used only when the System Time Source is Internal.