SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The transfer signal sequence for Freescale SPI format with SPO=0 and SPH=1 is shown in Figure 47-6, in which covers both single and continuous transfers.
Figure 47-6 Freescale SPI Frame Format
with SPO =0 and SPH=1
In this configuration, during idle periods:
If the SSI is enabled and valid data is in the transmit FIFO, the start of transmission is signified by the SSIFss master signal being driven low. The master SSITx output is then enabled. After an additional one-half SSIClk period, both master and slave valid data are enabled onto their respective transmission lines. At the same time, the SSIClk is enabled with a rising edge transition. Data is then captured on the falling edges and propagated on the rising edges of the SSIClk signal.
In the case of a single word transfer, after all bits have been transferred, the SSIFss line is returned to its idle high state one SSIClk period after the last bit has been captured.
For continuous back-to-back transfers, the SSIFss pin is held low between successive data words, and termination is the same as that of the single word transfer.