SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The TCP Segmentation Offload (TSO) engine is useful in offloading the TCP segmentation functions to the hardware. The TSO also supports UDP Segmentation Offload (USO) in which the UDP payload is segmented in the hardware. There are no sequencing/ordering controls available or updated in the segments, so the TSO can be used in point-to-point applications in which out of order packets are not expected by the receiver. The description and flow of TSO mentioned in this section is same as USO, any deviation is provided as notes.
In the TCP segmentation offload (TSO) feature, the DMA splits a large TCP packet into multiple small packets and passes these packets to the MTL as shown in Figure 43-14
Figure 43-14 TCP Segmentation Overview