SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Each proxy thread uses a simple state machine to track the currently usage by that host. This state machine is used to track when a proxy thread is in use or not, but also for error detection. The proxy thread always starts in idle state, when there is no currently activity. There is a write state for when the proxy thread has been written and contains data that has yet to be written to a resource. There is a read state for when the proxy thread has read data from a resource and that entire data has not been fully read by the host. When a proxy thread access completes, final write or final read, then the state will go back to idle. The following sections show the utilization of these states.