All interrupts that are generated by the R5FSS are
summarized in Module Integration, along with their mapping. They can be
divided into the following groups:
R5F CPU internal interrupts:
These are described in Arm Cortex-R5 Technical Reference Manual.
ECC аggregator interrupts: These
are described in the ECC Aggregator chapter.
RAT exception interrupt: This is
described in Section 7.3.2.6.