SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The Interrupt Aggregator (INTAGGR) provides a centralized machine which handles the termination of system events to that they can be coherently processed by the Host(s) in the system. Both the signaling and content of TI system events are incompatible with standard interrupt controllers. The INTAGGR provides mechanisms which convert the TI proprietary system events to standard level sensitive pending bits which can be used by all downstream interrupt infrastructure. Events can be presented to the INTAGGR in two different forms:
Events may be active high pulses, or clock synchronous rising edges, which are input on separate orthogonal pins. These are called 'Local Events'.
Local event signals that are used in pulse counting mode must be sourced by the same clock as the interrupt aggregator.
Local event signals that are used in edge counting mode must be sourced by pseudo-synchronous sources (and be a slower clock multiple) to the interrupt aggregator clock, and they must remain high for at least 1 'slow' clock cycle.
Events may be messages which are input in time division multiplexed sequential order from an Event Transport Lane. These are called 'Global Events'.
In both cases, these events need to be conditioned to transition them from a transient indicator that something occurred to a persistent and reliable indication of the current state of the system. The IA is architected to perform this conversion in an efficient and cost effective manner.