SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
Sample words are stored to memory in little-endian byte order, meaning that the least significant byte (LSByte) is stored at the lower byte address, and the most significant byte (MSByte) is stored at the higher byte address.
If both ADx pins are configured as input or both ADx pins are configured as output, the sample words for each audio channel are stored AD0 first and AD1 last.
Figure 25-6, Figure 25-7, Figure 25-8, Figure 25-9, and Figure 25-10 show examples of sample storage for typical use cases (F = frame index, C = channel index, P = ADx pin index).
Figure 25-6 16-Bit Mono I2S, LJF, and RJF Formats on One ADx Pin, Showing Six Frames in Memory
Figure 25-7 16-Bit Stereo I2S, LJF, and RJF Formats on One ADx Pin, Showing Three Frames in Memory
Figure 25-8 24-Bit Stereo I2S, LJF, and RJF Formats on One ADx Pin, Showing Two Frames in Memory
Figure 25-9 16-Bit I2S Format on AD0 and AD1 Pins, Showing Two Frames in Memory
Figure 25-10 16-Bit DSP Format on AD0 and AD1 Pins, Showing Two Frames in Memory