SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
The AUX Reference digital-to-analog converter (DAC) peripheral has the following features:
The primary application for the Reference DAC is to provide configurable references for the comparators in various power modes. Hence, the Reference DAC is often used together with other analog peripherals.
Figure 20-17 shows how the Reference DAC connects to analog nodes and to the digital interfaces.
Figure 20-17 Reference DAC Block Diagram