SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
There are two main event fabric blocks in the CC13x1x3 and CC26x1x3 devices. One in the MCU power domain (MCU event fabric) and the other in the AON power domain (AON event fabric). Figure 6-4 shows a simplified overview of the two modules together. The MCU event fabric is one of the subscribers to the AON event fabric.
Figure 6-4 Event Fabric Overview (Simplified)