SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
The following configuration is required to measure the time of high phase or low phase of an event source waveform. Use the sequence that follows:
Figure 20-5 illustrates a generic event source waveform.
Figure 20-5 Phase Width Timing Requirements
The phase to measure is labeled A, and it is arbitrarily set to the high phase of the event source in Figure 20-5. The opposite phase, which is not measured, is labeled B. Table 20-8 lists the timing requirements for both of these phases.
| Description | Label | Requirement | Condition |
|---|---|---|---|
| Minimum phase | t_minPhase | 292 ns | DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL = 0x0 |
| Minimum phase | t_minPhase | 230 ns | DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL = (0x1 | 0x2) |
| Minimum inverted-phase | t_minInvPhase | 126 ns | AUX_TDC:CTL.CMD = 0x1 |
| Minimum inverted-phase | t_minInvPhase | 42 ns | AUX_TDC:CTL.CMD = 0x2 |
If AUX_TDC:CTL.CMD = 0x2, the event source level must equal the level of inverted phase until AUX_TDC:STAT.STATE < 5. Failure to fulfill this requirement makes the TDC conversion start too late.