SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
In the idle-line multiprocessor protocol (ADDR/IDLE MODE bit = 0), blocks are separated by having a longer idle time between the blocks than between frames in the blocks. An idle time of ten or more high-level bits after a frame indicates the start of a new block. The time of a single bit is calculated directly from the baud value (bits per second). The idle-line multiprocessor communication format is shown in Figure 23-4 (ADDR/IDLE MODE bit is bit 3 of SCICCR).
Figure 23-4 Idle-Line
Multiprocessor Communication Format