SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
FILE: dcc_ex1_single_shot_verification.c
This program uses the XTAL clock as a reference clock to verify the frequency of the PLLRAW clock.
The Dual-Clock Comparator Module 0 is used for the clock verification. The clocksource0 is the reference clock (Fclk0 = 20Mhz) and the clocksource1 is the clock that needs to be verified (Fclk1 = 150Mhz). Seed is the value that gets loaded into the Counter.
Please refer to the TRM for details on counter seed values to be set.
External Connections
Watch Variables