SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
ISRs are similar to normal functions, but must do the following:
Requirements 1 and 3 are handled automatically by the TMS320C28x C compiler if the function is defined using the __interrupt keyword. For information on this keyword, see the Keywords section of the TMS320C28x Optimizing C/C++ Compiler v6.2.4 User's Guide. For information on writing assembly code to handle interrupts, see the Standard Operation for Maskable Interrupts section of the TMS320C28x CPU and Instruction Set Reference Guide.
The PIEACK bit for the interrupt group must be cleared manually in user code. This is normally done at the end of the ISR. If the PIEACK bit is not cleared, the CPU does not receive any further interrupts from that group. This does not apply to the Timer1 and Timer2 interrupts, which do not go through the PIE.