SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
Write accesses from the NPU module can be protected by setting the NPUWRPROTx bit of a specific register to 1. If a write access is done by the NPU module to protected memory, a write protection violation occurs.
If a write access is made to a dedicated or shared memory by the NPU module, and NPUWRPROTx is set to 1 for that memory, the write is called a NPU write protection violation.
A flag gets set in the NPU access violation flag register, and the memory address where the violation happened gets latched in the NPU fetch access violation address register. These are dedicated registers for each subsystem.
| Note 1: | All access protections are ignored during debug accesses. Write access to a protected memory go through when the write is done using the debugger, irrespective of the write protection configuration for that memory. |