SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
Table 10-120 lists the memory-mapped registers for the GPIO_DATA_READ_REGS registers. All register offset addresses not listed in Table 10-120 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | GPADAT_R | GPIO A Data Read Register | Go | |
| 2h | GPBDAT_R | GPIO B Data Read Register | Go | |
| 4h | GPCDAT_R | GPIO C Data Read Register | Go | |
| Ch | GPGDAT_R | GPIO G Data Read Register | Go | |
| Eh | GPHDAT_R | GPIO H Data Read Register | Go |
Complex bit access types are encoded to fit into small table cells. Table 10-121 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
GPADAT_R is shown in Figure 10-108 and described in Table 10-122.
Return to the Summary Table.
GPIO A Data Read Register.
Returns the contents of GPADAT register on a read, write to this register has no effect
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R | 0h | Returns the contents of what was written to the GPADAT register on a read, write to this register has no effect Reset type: CPU1.SYSRSn |
GPBDAT_R is shown in Figure 10-109 and described in Table 10-123.
Return to the Summary Table.
GPIO B Data Read Register.
Returns the contents of GPBDAT register on a read, write to this register has no effect
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R | 0h | Returns the contents of what was written to the GPBDAT register on a read, write to this register has no effect Reset type: CPU1.SYSRSn |
GPCDAT_R is shown in Figure 10-110 and described in Table 10-124.
Return to the Summary Table.
GPIO C Data Read Register.
Returns the contents of GPCDAT register on a read, write to this register has no effect
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R | 0h | Returns the contents of what was written to the GPCDAT register on a read, write to this register has no effect Reset type: CPU1.SYSRSn |
GPGDAT_R is shown in Figure 10-111 and described in Table 10-125.
Return to the Summary Table.
GPIO G Data Read Register.
Returns the contents of GPGDAT register on a read, write to this register has no effect
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R | 0h | Returns the contents of what was written to the GPGDAT register on a read, write to this register has no effect Reset type: CPU1.SYSRSn |
GPHDAT_R is shown in Figure 10-112 and described in Table 10-126.
Return to the Summary Table.
GPIO H Data Read Register.
Returns the contents of GPHDAT register on a read, write to this register has no effect
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R | 0h | Returns the contents of what was written to the GPHDAT register on a read, write to this register has no effect Reset type: CPU1.SYSRSn |