SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
The best way to understand how to use the HRPWM capabilities is through two real examples:
The following examples all have initialization and configuration code written in C. To make these easier to understand, the #defines shown below are used.
Example19-2 assumes MEP step size of 150ps and does not use the SFO library.