SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
This section explains how the boot mode select pins are customized by the user, by programming the BOOTPIN-CONFIG location (refer to Table 4-6) in the user-configurable dual-zone security module (DCSM) OTP. The location in the DCSM OTP is Z1-OTP-BOOTPIN-CONFIG or Z2-OTP-BOOTPIN-CONFIG. When debugging, EMU-BOOTPIN-CONFIG is the emulation equivalent of Z1-OTP-BOOTPIN-CONFIG/Z2-OTP-BOOTPIN-CONFIG, and can be programmed to experiment with different boot modes without writing to OTP. The device can be programmed to use zero, one, two or three boot mode select pins as needed.
| Bit | Name | Description |
|---|---|---|
| 31:24 | Key | Write 0x5A to these 8-bits to tell the boot ROM code that the bits in this register are valid. |
| 23:16 | Boot Mode Select Pin 2 (BMSP2) | Refer to BMSP0 description. |
| 15:8 | Boot Mode Select Pin 1 (BMSP1) | Refer to BMSP0 description. |
| 7:0 | Boot Mode Select Pin 0 (BMSP0) |
Set to the GPIO pin to be used during boot (up to 255). 0x0 = GPIO0 0x01 = GPIO1, and so on. Writing 0xFF disables this BMSP and this pin is no longer used to select the boot mode. |
| BOOTPIN_CONFIG Key |
BMSP0 | BMSP1 | BMSP2 | Realized Boot Mode |
|---|---|---|---|---|
| != 0x5A | Don’t Care | Don’t Care | Don’t Care | Boot as defined by the factory default BMSPs |
| = 0x5A | 0xFF | 0xFF | 0xFF | Boot as defined in the boot table for boot mode 0 (All BMSPs disabled) |
| Valid GPIO | 0xFF | 0xFF | Boot as defined by the value of BMSP0 (BMSP1 and BMSP2 disabled) |
|
| 0xFF | Valid GPIO | 0xFF | Boot as defined by the value of BMSP1 (BMSP0 and BMSP2 disabled) |
|
| 0xFF | 0xFF | Valid GPIO | Boot as defined by the value of BMSP2 (BMSP0 and BMSP1 disabled) |
|
| Valid GPIO | Valid GPIO | 0xFF | Boot as defined by the values of BMSP0 and BMSP1 (BMSP2 disabled) |
|
| Valid GPIO | 0xFF | Valid GPIO | Boot as defined by the values of BMSP0 and BMSP2 (BMSP1 disabled) |
|
| 0xFF | Valid GPIO | Valid GPIO | Boot as defined by the values of BMSP1 and BMSP2 (BMSP0 disabled) |
|
| Valid GPIO | Valid GPIO | Valid GPIO | Boot as defined by the values of BMSP0, BMSP1, and BMSP2 | |
| Invalid GPIO | Valid GPIO | Valid GPIO | BMSP0 is reset to the factory default BMSP0 GPIO Boot as defined by the values of BMSP0, BMSP1, and BMSP2 |
|
| Valid GPIO | Invalid GPIO | Valid GPIO | BMSP1 is reset to the factory default BMSP1 GPIO Boot as defined by the values of BMSP0, BMSP1, and BMSP2 |
|
| Valid GPIO | Valid GPIO | Invalid GPIO | BMSP2 is reset to the factory default state, which is disabled Boot as defined by the values of BMSP0 and BMSP1 |