SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
In restricted operation mode, the CAN node is able to receive data and remote frames and to give acknowledgment to valid frames, but the node does not send data frames, remote frames, active error frames, or overload frames. In case of an error condition or overload condition, the node does not send dominant bits; instead the node waits for the occurrence of bus idle condition to resynchronize to the CAN communication. The receive and transmit error counters (MCAN_ECR.REC and MCAN_ECR.TEC) are frozen while CAN error logging (MCAN_ECR.CEL) is active. The Host CPU can set the MCAN module into Restricted Operation Mode by setting the MCAN_CCCR.ASM bit. The bit can only be set by the Host CPU at any time when both MCAN_CCCR.CCE and MCAN_CCCR.INIT bits are set to 1.
The restricted operation mode is automatically entered when the Tx Handler is not able to read data from the Message RAM in time. To leave restricted operation mode, the Host CPU has to reset the MCAN_CCCR.ASM bit. This mode can be used in applications that adapt themselves to different CAN bit rates. In this case, the application tests different bit rates and leaves the restricted operation mode after the node has received a valid frame.