SPRUJ53C April 2024 – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
FILE: i2c_ex6_eeprom_interrupt.c
This program will shows how to perform different EEPROM write and read commands using I2C interrupts EEPROM used for this example is AT24C256
External Connections
SCL | DEVICE_GPIO_PIN_SCLA | SCL SDA | DEVICE_GPIO_PIN_SDAA | SDA
Make sure to connect GND pins if EEPROM and C2000 device are in different board.//Example 1: EEPROM Byte Write //Example 2: EEPROM Byte Read //Example 3: EEPROM word (16-bit) write //Example 4: EEPROM word (16-bit) read //Example 5: EEPROM Page write //Example 6: EEPROM word Paged read
Watch Variables