SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
There are two main event fabric blocks in the CC13x4x10 and CC26x4x10 devices. One in the MCU power domain (MCU event fabric) and the other in the AON power domain (AON event fabric). Figure 5-2 shows a simplified overview of the two modules together. The MCU event fabric is one of the subscribers to the AON event fabric.
The AUX Domain Sensor Controller and peripherals has an internal simplified event fabric for routing of events internally and as inputs to the AON event fabric and MCU event fabric. See Section 20.6 for details.