SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
This section provides an overview of the Sensor Controller Engine CPU core. For most users, this information can provide an understanding of the Sensor Controller Engine’s capabilities and limitations, and also be used as a reference when debugging Sensor Controller tasks.
There is normally no need to write any assembly code for the Sensor Controller. It is possible to create your own task resources and procedures for the Sensor Controller Studio if needed, for example, when: