SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The COMPA positive input can connect to:
The reference DAC output connection is not intended for COMPA usage. Hence, the connection shows as dotted in Figure 20-30.
The user must ensure that the positive input of the COMPA peripheral has only one driver at all times. To avoid shorting signals together internally, TI provides ROM-based functions that ensure a break-before-make switching of the internal muxes.