SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
There are a few cases which can occur when processing TRs which are not considered errors but which will require handling in order to avoid locking up the UTC read or write engines. Since the UTC performs transfer sequencing using a count based mechanism it is susceptible to becoming out of synchronization if the source of the data and the destination for the data do not exactly match in their expectations for how much data will be transferred. The following outline these scenarios.