SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
If a param defines a maximum outstanding read data byte count, then this function will track the requested read bytes against the limit. If a read command does not violate the total read bytes outstanding limit then the read is allowed to the VBUSM.C, otherwise it is stalled. When read data arrives from the VBUSM.C the outstanding count is reduced, allowing more read commands to be sent.