SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
Table 12-4147 lists some of the I/Os of the GPMC module.
| Module Pin | I/O(1) | Description |
|---|---|---|
| GPMC0_FCLK | Internal | Functional clock. Acts as the time reference. |
| GPMC0_ICLK | Internal | Interface clock. Acts as the time reference. |
| GPMC0_CLKOUT | O | External clock provided to the external device for synchronous operations |
| GPMC0_A[21-16] | O | Address |
| GPMC0_AD[15-0] | I/O | Data-multiplexed with addresses A[16-1] on memory side |
| GPMC0_CSn[3-0] | O | Chip-selects |
| GPMC0_ADVn_ALE | O | Address valid enable |
| GPMC0_OEn_REn | O | Output enable (read access only) |
| GPMC0_WEn | O | Write enable (write access only) |
| GPMC0_WAIT[1-0] | I | Ready signal from memory device. Indicates when valid burst data is ready to be read |
Figure 12-2116 shows the typical connection between the GPMC module and an attached NOR Flash memory.
The following sections demonstrate how to calculate GPMC parameters for three access types: