SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
Figure 12-138 illustrates the dead-band generator submodule within the EPWM module.
Figure 12-2632 Dead-Band Generator SubmoduleThe "Action-qualifier (AQ) Module" section discussed how it is possible to generate the required dead-band by having full control over edge placement using both the CMPA and CMPB resources of the EPWM module. However, if the more classical edge delay-based dead-band with polarity control is required, then the dead-band generator submodule should be used.
The key functions of the dead-band generator submodule are: