SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
A faulted transaction will have the flush bit set on the outgoing transaction so that it will return errors by the interconnect. The atype will be set to 0 since the memory attributes have not been replaced. And the outgoing transaction address will have the upper bits set to the fault_addr parameter value (see Section 8.3.1.2), which defines an interconnect address that will always return errors and not interfere with any valid slave traffic (such as to memory).