SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
The CRC aware SPI transfer can be performed when both controller and device are configured to work in the Octal DDR Protocol.
For write transactions (the controller transmits data throughout all transfer), the controller is responsible for sending address CRC byte (XOR of all address bytes) following address bytes and TX data CRC byte (XOR of all data bytes to write) following data chunk with size as defined in OSPI_MODE_BIT_CONFIG_REG[10-8] CHUNK_SIZE_FLD bit field. All CRC data are being calculated and sent automatically by the controller and the external device is responsible for reacting accordingly on any possible interpolation on the Flash interface. For read transactions, the controller is also responsible for sending address CRC byte (like for write) and for getting and progressing RX data CRC byte returning by the Flash Device after each chunk with size as defined in OSPI_MODE_BIT_CONFIG_REG[10-8] CHUNK_SIZE_FLD bit field. At the time when the Flash Device is returning data back to the controller, the controller dynamically calculates checksum byte by byte. Once the chunk is completed, CRC returned from Flash Device should fit to dynamically calculated CRC by the controller. In case of any deviation, controller reports CRC error to the system by corresponding interrupt (CRC error interrupt). The controller also provides the last captured CRC data in RX data chunk (defined in OSPI_MODE_BIT_CONFIG_REG[31-24] RX_CRC_DATA_LOW_FLD and OSPI_MODE_BIT_CONFIG_REG[23-16] RX_CRC_DATA_UP_FLD bit fields) to give the software driver the opportunity to further detecting any data corruption on system interfaces. The CRC data valid interrupt informs the system about the accessibility of the new RX CRC data in the registers. Once the system gets the full data word, it can calculate CRC by itself. At the time it collects all data words in chunk and then gets the CRC data valid interrupt, it can compare these data and react accordingly.
Some devices also have embedded ECC mechanism allowing them to report data abnormal conditions on their ECC Correction Signal output. At the time this output turns low, the device expect the OSPI controller to read status register of the device in order to get more details about the source of detected abnormal situation. The OSPI controller investigates ECC status on its ECC_FAIL input and generates an interrupt when detecting this signal being low.