SLUUCI8 November 2023 BQ76905
The BQ76905 integrates an extensive protection subsystem which can monitor a variety of parameters, initiate protective actions, and autonomously recover based on conditions. The device also includes a wide range of flexibility, such that the device can be configured to monitor and initiate protective action, but with recovery controlled by the host processor, or such that the device only monitors and alerts the host processor whenever conditions warrant protective action, but with action and recovery fully controlled by the host processor. The protection subsystem includes a suite of individual protections that can be individually enabled and configured, as shown in Table 6-1. The current protections are based on comparator thresholds, while most voltage and temperature protections are based on ADC measurements. Some protection checks are primarily for diagnostic purposes, so the device can be autonomously disabled if a malfunction is detected. The device integrates NFET drivers for low-side CHG and DSG protection FETs, which can be configured in a series or parallel configuration. The FET drivers also support PWM modes of operation, which can be used to implement a precharge or predischarge functionality.
| Protection | Implementation | Description |
|---|---|---|
| Cell Undervoltage | ADC measurement | Detects individual cell voltage below programmed threshold |
| Cell Overvoltage | ADC measurement | Detects individual cell voltage above programmed threshold |
| Overcurrent in Charge | Analog comparator | Detects charging current above programmed threshold |
| Overcurrent in Discharge 1 / 2 | Analog comparator | Two levels of detection for discharging current beyond programmed thresholds |
| Short Circuit in Discharge | Analog comparator | Detects discharging current above programmed threshold |
| Undertemperature in Charge | ADC measurement | Detects thermistor temperature below programmed threshold limit for charging operation |
| Overtemperature in Charge | ADC measurement | Detects thermistor temperature above programmed threshold limit for charging operation |
| Undertemperature in Discharge | ADC measurement | Detects thermistor temperature below programmed threshold limit for discharging operation |
| Overtemperature in Discharge | ADC measurement | Detects thermistor temperature above programmed threshold limit for discharging operation |
| Internal Overtemperature | ADC measurement | Detects internal device temperature above programmed threshold |
| REGOUT LDO Check | Analog comparator | Diagnostic check - detects voltage or temperature fault on REGOUT regulator when enabled |
| Voltage Reference Check | ADC measurement | Diagnostic check which digitizes the internal 1.8V LDO using the ADC and VREF1, and detects any excessive deviation from the expected result |
| VSS Check | ADC measurement | Diagnostic check on ADC mux - device digitizes VSS and detects any excessive deviation from the expected result |
| Host Watchdog | Digital logic | Detects absence of host processor communications |
The individual protections are enabled by setting the related Settings:Protection:Enabled Protections A – B data memory configuration registers. Most protections include a programmable threshold, and when the monitored parameter first exceeds the programmed threshold, a protection alert is asserted. After the parameter remains beyond the threshold for a programmable delay period, a protection status fault is asserted (and the alert is deasserted). The protection alerts are provided by the 0x02 Safety Alert A() and 0x04 Safety Alert B() commands, while the protection status faults are provided by the 0x03 Safety Status A() and 0x05 Safety Status B() commands, as shown below. Most protections also include a programmable recovery criteria, such that if the parameter no longer exceeds the threshold by some margin, the protection status fault is deasserted. Protection alert and status faults can be mapped to provide an interrupt to the host processor on the ALERT pin, using the 0x62 Alarm Status(), 0x64 Alarm Raw Status(), and 0x66 Alarm Enable() commands.
| Bit | Name | Description |
|---|---|---|
| 7 | COV | Cell Overvoltage Safety Alert |
| 6 | CUV | Cell Undervoltage Safety Alert |
| 5 | SCD | Short Circuit in Discharge Safety Alert |
| 4 | OCD1 | Overcurrent in Discharge 1 Safety Alert |
| 3 | OCD2 | Overcurrent in Discharge 2 Safety Alert |
| 2 | OCC | Overcurrent in Charge Safety Alert |
| 1-0 | RSVD0 | Reserved |
| Bit | Name | Description |
|---|---|---|
| 7 | COV | Cell Overvoltage Safety Fault |
| 6 | CUV | Cell Undervoltage Safety Fault |
| 5 | SCD | Short Circuit in Discharge Safety Fault |
| 4 | OCD1 | Overcurrent in Discharge 1 Safety Fault |
| 3 | OCD2 | Overcurrent in Discharge 2 Safety Fault |
| 2 | OCC | Overcurrent in Charge Safety Fault |
| 1 | CURLATCH | Current Protection Latch Safety Fault |
| 0 | REGOUT | REGOUT Safety Fault |
| Bit | Name | Description |
|---|---|---|
| 7 | OTD | Overtemperature in Discharge Safety Alert |
| 6 | OTC | Overtemperature in Charge Safety Alert |
| 5 | UTD | Undertemperature in Discharge Safety Alert |
| 4 | UTC | Undertemperature in Charge Safety Alert |
| 3 | OTINT | Internal Overtemperature Safety Alert |
| 2 | HWD | Host Watchdog Safety Alert |
| 1 | VREF | VREF Measurement Diagnostic Alert |
| 0 | VSS | VSS Measurement Diagnostic Alert |
| Bit | Name | Description |
|---|---|---|
| 7 | OTD | Overtemperature in Discharge Safety Fault |
| 6 | OTC | Overtemperature in Charge Safety Fault |
| 5 | UTD | Undertemperature in Discharge Safety Fault |
| 4 | UTC | Undertemperature in Charge Safety Fault |
| 3 | OTINT | Internal Overtemperature Safety Fault |
| 2 | HWD | Host Watchdog Safety Fault |
| 1 | VREF | VREF Measurement Diagnostic Fault |
| 0 | VSS | VSS Measurement Diagnostic Fault |
The thresholds, delays, and recovery criteria are controlled by individual data memory settings in the Protections class. For example, the Cell Undervoltage Protection is configured using the Protections:Cell Voltage:Cell Undervoltage Protection Threshold, Protections:Cell Voltage:Cell Undervoltage Protection Delay, and Protections:Cell Voltage:Cell Undervoltage Protection Recovery Hysteresis data memory settings.
The control of the protection FETs in response to a detected protection event is also configurable, with the device able to operate in a fully autonomous mode, a completely manual mode (controlled through host commands over the serial communications bus), or a combination of the two. Autonomous mode is enabled by setting the Settings:Configuration:FET Options[FET_EN] data memory configuration bit or sending the 0x0022 FET Enable() subcommand, which toggles the [FET_EN] bit. The device can operate in a combined autonomous/manual mode, such that the device can operate autonomously when the host processor does not intervene, but still allows the host to override the autonomous decisions and force FETs on or off based on serial communications. This can be attractive in cases where the host needs autonomous reaction to selected faults, such as a short circuit in discharge event, to provide the fastest protection response, but prefer manual control for other faults, such as cell overtemperature or overvoltage faults. The 0x29 FET Control() command provides manual FET control capability by the host. If the user is concerned about unauthorized or inadvertent manual FET control by a host, these selected commands can be disabled using the Settings:Configuration:FET Options[HOST_FETOFF_EN] and [HOST_FETON_EN] data memory configuration settings. Each protection can be configured whether it autonomously disables the pertinent protection FET using the Settings:Protection:CHG FET Protections A, Settings:Protection:DSG FET Protections A, and Settings:Protection:Both FET Protections C settings.