SLUUB65B May 2015 – December 2022
Clears an Imax interrupt that is presently asserted on the (SE or HDQ) pin. The command is only applicable if the Imax feature is enabled in Pack Configuration D [IMAXEN].