SLUUB65B May 2015 – December 2022
The following flowchart demonstrates how the host system obtains the raw data to calibrate current, voltage, and temperature. The host system uses this flow in conjunction with the Current, Voltage, and Temperature flows described in this appendix. It is recommended that the host system samples the raw data multiple times at a rate of once per second to obtain an average of the raw current, voltage, and temperature. The host system needs to make sure the fuel gauge is UNSEALED.
The step labeled Enter CALIBRATION Mode refers to Section 18.3, Enter CALIBRATION Mode.
The step labeled Exit CALIBRATION Mode refers to Section 18.4, Exit CALIBRATION Mode.