SLUUB65B May 2015 – December 2022
Use MAC commands for CC Offset calibration. The host system does not need to write information to the data flash (DF). See Section 16.1.1.1 for the description of the CONTROL_STATUS[CCA] bit. The host system needs to make sure the fuel gauge is UNSEALED.
While the device is calibrating the CC Offset, the host system must not read the CONTROL_STATUS register at a rate greater than once every 0.5 seconds.
The step labeled Enter CALIBRATION Mode refers to Section 18.3, Enter CALIBRATION Mode.
The step labeled Exit CALIBRATION Mode refers to Section 18.4, Exit CALIBRATION Mode.