SLUUB65B May 2015 – December 2022
Int Temp Offset is used to calibrate offset errors in the measurement of the reported Temperature() if the internal temperature sensor is used. The gain of the internal temperature sensor is accurate enough that a calibration for gain is not required. Ext Temp Offset is for calibrating the offset of the thermistor connected to the TS1 pin of the fuel gauge as reported by Temperature(). The gain of the thermistor is accurate enough that a calibration for gain is not required.