ZHCSII3E August 2016 – July 2018
PRODUCTION DATA.
Table 4-1 describes the terminal characteristics and the signals multiplexed on each ball. The following list describes the table column headers:
NOTE
Table 4-1 does not take into account the subsystem multiplexing signals. Subsystem multiplexing signals are described in Section 4.3, Signal Descriptions.
NOTE
In driver off mode, the buffer is configured in high-impedance.
NOTE
In some cases Table 4-1 may present more than one signal name per muxmode for the same ball. First signal in the list is the dominant function as selected via CTRL_CORE_PAD_* register.
All other signals are virtual functions that present alternate multiplexing options. This virtual functions are controlled via CTRL_CORE_ALT_SELECT_MUX or CTRL_CORE_VIP_MUX_SELECT register. For more information on how to use this options, please refer to Device TRM, Chapter Control Module, Section Pad Configuration Registers.
NOTE
The default mode is the mode at the release of the reset; also see the RESET REL. MUXMODE column.
NOTE
For more information on the CORE_PWRON_RET_RST reset signal and its reset sources, see the Power, Reset, and Clock Management / PRCM Reset Management Functional Description section of the Device TRM.
NOTE
For more information, see the hysteresis values in Section 5.7, Electrical Characteristics.
NOTE
For programmable buffer strength:
NOTE
Configuring two pins to the same input signal is not supported as it can yield unexpected results. This can be easily prevented with the proper software configuration (Hi-Z mode is not an input signal).
NOTE
When a pad is set into a multiplexing mode which is not defined by pin multiplexing, that pad’s behavior is undefined. This should be avoided.
NOTE
Some of the EMIF1 signals have an additional state change at the release of porz. The state that the signals change to at the release of porz is as follows:
drive 0 (OFF) for: ddr1_ck, ddr1_odt[0], ddr1_rst.
drive 1 (OFF) for: ddr1_casn, ddr1_rasn, ddr1_wen, ddr1_nck, ddr1_ba[2:0], ddr1_a[15:0], ddr1_csn[0], ddr1_cke, ddr1_dqm[3:0]
NOTE
Dual rank support is not available on this device, but signal names are retained for consistency with the TDA2xx family of devices.
| BALL NUMBER [1] | BALL NAME [2] | SIGNAL NAME [3] | MUXMODE [4] | TYPE [5] | BALL RESET STATE [6] | BALL RESET REL. STATE [7] | BALL RESET REL. MUXMODE [8] | I/O VOLTAGE VALUE [9] | POWER [10] | HYS [11] | BUFFER TYPE [12] | PULL UP/DOWN TYPE [13] | DSIS [14] |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| F8 | cap_vbbldo_dsp | cap_vbbldo_dsp | CAP | ||||||||||
| T7 | cap_vbbldo_gpu | cap_vbbldo_gpu | CAP | ||||||||||
| G14 | cap_vbbldo_iva | cap_vbbldo_iva | CAP | ||||||||||
| F17 | cap_vbbldo_mpu | cap_vbbldo_mpu | CAP | ||||||||||
| U20 | cap_vddram_core1 | cap_vddram_core1 | CAP | ||||||||||
| K7 | cap_vddram_core3 | cap_vddram_core3 | CAP | ||||||||||
| G19 | cap_vddram_core4 | cap_vddram_core4 | CAP | ||||||||||
| L7 | cap_vddram_dsp | cap_vddram_dsp | CAP | ||||||||||
| V7 | cap_vddram_gpu | cap_vddram_gpu | CAP | ||||||||||
| G12 | cap_vddram_iva | cap_vddram_iva | CAP | ||||||||||
| G18 | cap_vddram_mpu | cap_vddram_mpu | CAP | ||||||||||
| AC1 | csi2_0_dx0 | csi2_0_dx0 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| AD1 | csi2_0_dx1 | csi2_0_dx1 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| AE2 | csi2_0_dx2 | csi2_0_dx2 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| AB2 | csi2_0_dy0 | csi2_0_dy0 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| AC2 | csi2_0_dy1 | csi2_0_dy1 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| AD2 | csi2_0_dy2 | csi2_0_dy2 | 0 | I | 1.8 | Yes | LVCMOS CSI2 | PU/PD | |||||
| H23 | dcan1_rx | dcan1_rx | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart8_txd | 2 | O | |||||||||||
| mmc2_sdwp | 3 | I | 0 | ||||||||||
| hdmi1_cec | 6 | IO | |||||||||||
| gpio1_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H22 | dcan1_tx | dcan1_tx | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart8_rxd | 2 | I | 1 | ||||||||||
| mmc2_sdcd | 3 | I | 1 | ||||||||||
| hdmi1_hpd | 6 | IO | |||||||||||
| gpio1_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AC18 | ddr1_a0 | ddr1_a0 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE19 | ddr1_a1 | ddr1_a1 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD19 | ddr1_a2 | ddr1_a2 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB19 | ddr1_a3 | ddr1_a3 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD20 | ddr1_a4 | ddr1_a4 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE20 | ddr1_a5 | ddr1_a5 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA18 | ddr1_a6 | ddr1_a6 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA20 | ddr1_a7 | ddr1_a7 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| Y21 | ddr1_a8 | ddr1_a8 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC20 | ddr1_a9 | ddr1_a9 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA21 | ddr1_a10 | ddr1_a10 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC21 | ddr1_a11 | ddr1_a11 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC22 | ddr1_a12 | ddr1_a12 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC15 | ddr1_a13 | ddr1_a13 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB15 | ddr1_a14 | ddr1_a14 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC16 | ddr1_a15 | ddr1_a15 | 0 | O | PD | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE16 | ddr1_ba0 | ddr1_ba0 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA16 | ddr1_ba1 | ddr1_ba1 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB16 | ddr1_ba2 | ddr1_ba2 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD16 | ddr1_casn | ddr1_casn | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD21 | ddr1_ck | ddr1_ck | 0 | O | PD | drive 0 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB18 | ddr1_cke | ddr1_cke | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC19 | ddr1_csn0 | ddr1_csn0 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA23 | ddr1_d0 | ddr1_d0 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC24 | ddr1_d1 | ddr1_d1 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB24 | ddr1_d2 | ddr1_d2 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD24 | ddr1_d3 | ddr1_d3 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB23 | ddr1_d4 | ddr1_d4 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC23 | ddr1_d5 | ddr1_d5 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD23 | ddr1_d6 | ddr1_d6 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE24 | ddr1_d7 | ddr1_d7 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA24 | ddr1_d8 | ddr1_d8 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| W25 | ddr1_d9 | ddr1_d9 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| Y23 | ddr1_d10 | ddr1_d10 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD25 | ddr1_d11 | ddr1_d11 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AC25 | ddr1_d12 | ddr1_d12 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AB25 | ddr1_d13 | ddr1_d13 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AA25 | ddr1_d14 | ddr1_d14 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| W24 | ddr1_d15 | ddr1_d15 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| W23 | ddr1_d16 | ddr1_d16 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| U25 | ddr1_d17 | ddr1_d17 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| U24 | ddr1_d18 | ddr1_d18 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| W21 | ddr1_d19 | ddr1_d19 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| T22 | ddr1_d20 | ddr1_d20 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| U22 | ddr1_d21 | ddr1_d21 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| U23 | ddr1_d22 | ddr1_d22 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| T21 | ddr1_d23 | ddr1_d23 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| T23 | ddr1_d24 | ddr1_d24 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| T25 | ddr1_d25 | ddr1_d25 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| T24 | ddr1_d26 | ddr1_d26 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| P21 | ddr1_d27 | ddr1_d27 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| N21 | ddr1_d28 | ddr1_d28 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| P22 | ddr1_d29 | ddr1_d29 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| P23 | ddr1_d30 | ddr1_d30 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| P24 | ddr1_d31 | ddr1_d31 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE23 | ddr1_dqm0 | ddr1_dqm0 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| W22 | ddr1_dqm1 | ddr1_dqm1 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| U21 | ddr1_dqm2 | ddr1_dqm2 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| P25 | ddr1_dqm3 | ddr1_dqm3 | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD22 | ddr1_dqs0 | ddr1_dqs0 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| Y24 | ddr1_dqs1 | ddr1_dqs1 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| V24 | ddr1_dqs2 | ddr1_dqs2 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| R24 | ddr1_dqs3 | ddr1_dqs3 | 0 | IO | PD | PD | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| AE22 | ddr1_dqsn0 | ddr1_dqsn0 | 0 | IO | PU | PU | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| Y25 | ddr1_dqsn1 | ddr1_dqsn1 | 0 | IO | PU | PU | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| V25 | ddr1_dqsn2 | ddr1_dqsn2 | 0 | IO | PU | PU | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| R25 | ddr1_dqsn3 | ddr1_dqsn3 | 0 | IO | PU | PU | 1.35/1.5 | vdds_ddr1 | LVCMOS DDR | PUx/PDy | |||
| AE21 | ddr1_nck | ddr1_nck | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD18 | ddr1_odt0 | ddr1_odt0 | 0 | O | PD | drive 0 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AD17 | ddr1_rasn | ddr1_rasn | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| AE17 | ddr1_rst | ddr1_rst | 0 | O | PD | drive 0 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| Y20 | ddr1_vref0 | ddr1_vref0 | 0 | PWR | OFF | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | |||
| AE18 | ddr1_wen | ddr1_wen | 0 | O | PU | drive 1 (OFF) | 1.35/1.5 | vdds_ddr1 | No | LVCMOS DDR | PUx/PDy | ||
| C21 | emu0 | emu0 | 0 | IO | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio8_30 | 14 | IO | |||||||||||
| C22 | emu1 | emu1 | 0 | IO | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio8_31 | 14 | IO | |||||||||||
| E14 | emu2 | emu2 | 2 | O | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| F14 | emu3 | emu3 | 2 | O | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| F13 | emu4 | emu4 | 2 | O | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| Y5 | gpio6_10 | gpio6_10 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mdio_mclk | 1 | O | 1 | ||||||||||
| i2c3_sda | 2 | IO | 1 | ||||||||||
| usb3_ulpi_d7 | 3 | IO | 0 | ||||||||||
| vin2b_hsync1 | 4 | I | |||||||||||
| vin1a_clk0 | 9 | I | 0 | ||||||||||
| ehrpwm2A | 10 | O | |||||||||||
| gpio6_10 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y6 | gpio6_11 | gpio6_11 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mdio_d | 1 | IO | 1 | ||||||||||
| i2c3_scl | 2 | IO | 1 | ||||||||||
| usb3_ulpi_d6 | 3 | IO | 0 | ||||||||||
| vin2b_vsync1 | 4 | I | |||||||||||
| vin1a_de0 | 9 | I | 0 | ||||||||||
| ehrpwm2B | 10 | O | |||||||||||
| gpio6_11 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H21 | gpio6_14 | gpio6_14 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp1_axr8 | 1 | IO | 0 | ||||||||||
| dcan2_tx | 2 | IO | 1 | ||||||||||
| uart10_rxd | 3 | I | 1 | ||||||||||
| i2c3_sda | 9 | IO | 1 | ||||||||||
| timer1 | 10 | IO | |||||||||||
| gpio6_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K22 | gpio6_15 | gpio6_15 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp1_axr9 | 1 | IO | 0 | ||||||||||
| dcan2_rx | 2 | IO | 1 | ||||||||||
| uart10_txd | 3 | O | |||||||||||
| i2c3_scl | 9 | IO | 1 | ||||||||||
| timer2 | 10 | IO | |||||||||||
| gpio6_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K23 | gpio6_16 | gpio6_16 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp1_axr10 | 1 | IO | 0 | ||||||||||
| clkout1 | 9 | O | |||||||||||
| timer3 | 10 | IO | |||||||||||
| gpio6_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| M1 | gpmc_a0 | gpmc_a0 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d16 | 2 | I | 0 | ||||||||||
| vout3_d16 | 3 | O | |||||||||||
| vin1b_d0 | 6 | I | 0 | ||||||||||
| i2c4_scl | 7 | IO | 1 | ||||||||||
| uart5_rxd | 8 | I | 1 | ||||||||||
| gpio7_3
gpmc_a26 gpmc_a16 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| M2 | gpmc_a1 | gpmc_a1 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d17 | 2 | I | 0 | ||||||||||
| vout3_d17 | 3 | O | |||||||||||
| vin1b_d1 | 6 | I | 0 | ||||||||||
| i2c4_sda | 7 | IO | 1 | ||||||||||
| uart5_txd | 8 | O | |||||||||||
| gpio7_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L2 | gpmc_a2 | gpmc_a2 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d18 | 2 | I | 0 | ||||||||||
| vout3_d18 | 3 | O | |||||||||||
| vin1b_d2 | 6 | I | 0 | ||||||||||
| uart7_rxd | 7 | I | 1 | ||||||||||
| uart5_ctsn | 8 | I | 1 | ||||||||||
| gpio7_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L1 | gpmc_a3 | gpmc_a3 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_cs2 | 1 | O | 1 | ||||||||||
| vin1a_d19 | 2 | I | 0 | ||||||||||
| vout3_d19 | 3 | O | |||||||||||
| vin1b_d3 | 6 | I | 0 | ||||||||||
| uart7_txd | 7 | O | |||||||||||
| uart5_rtsn | 8 | O | |||||||||||
| gpio7_6 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K3 | gpmc_a4 | gpmc_a4 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_cs3 | 1 | O | 1 | ||||||||||
| vin1a_d20 | 2 | I | 0 | ||||||||||
| vout3_d20 | 3 | O | |||||||||||
| vin1b_d4 | 6 | I | 0 | ||||||||||
| i2c5_scl | 7 | IO | 1 | ||||||||||
| uart6_rxd | 8 | I | 1 | ||||||||||
| gpio1_26 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K2 | gpmc_a5 | gpmc_a5 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d21 | 2 | I | 0 | ||||||||||
| vout3_d21 | 3 | O | |||||||||||
| vin1b_d5 | 6 | I | 0 | ||||||||||
| i2c5_sda | 7 | IO | 1 | ||||||||||
| uart6_txd | 8 | O | |||||||||||
| gpio1_27 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| J1 | gpmc_a6 | gpmc_a6 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d22 | 2 | I | 0 | ||||||||||
| vout3_d22 | 3 | O | |||||||||||
| vin1b_d6 | 6 | I | 0 | ||||||||||
| uart8_rxd | 7 | I | 1 | ||||||||||
| uart6_ctsn | 8 | I | 1 | ||||||||||
| gpio1_28 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K1 | gpmc_a7 | gpmc_a7 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_d23 | 2 | I | 0 | ||||||||||
| vout3_d23 | 3 | O | |||||||||||
| vin1b_d7 | 6 | I | 0 | ||||||||||
| uart8_txd | 7 | O | |||||||||||
| uart6_rtsn | 8 | O | |||||||||||
| gpio1_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K4 | gpmc_a8 | gpmc_a8 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_hsync0 | 2 | I | 0 | ||||||||||
| vout3_hsync | 3 | O | |||||||||||
| vin1b_hsync1 | 6 | I | 0 | ||||||||||
| timer12 | 7 | IO | |||||||||||
| spi4_sclk | 8 | IO | 0 | ||||||||||
| gpio1_30 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H1 | gpmc_a9 | gpmc_a9 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_vsync0 | 2 | I | 0 | ||||||||||
| vout3_vsync | 3 | O | |||||||||||
| vin1b_vsync1 | 6 | I | 0 | ||||||||||
| timer11 | 7 | IO | |||||||||||
| spi4_d1 | 8 | IO | 0 | ||||||||||
| gpio1_31 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| J2 | gpmc_a10 | gpmc_a10 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_de0 | 2 | I | 0 | ||||||||||
| vout3_de | 3 | O | |||||||||||
| vin1b_clk1 | 6 | I | 0 | ||||||||||
| timer10 | 7 | IO | |||||||||||
| spi4_d0 | 8 | IO | 0 | ||||||||||
| gpio2_0 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L3 | gpmc_a11 | gpmc_a11 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin1a_fld0 | 2 | I | 0 | ||||||||||
| vout3_fld | 3 | O | |||||||||||
| vin1b_de1 | 6 | I | 0 | ||||||||||
| timer9 | 7 | IO | |||||||||||
| spi4_cs0 | 8 | IO | 1 | ||||||||||
| gpio2_1 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G1 | gpmc_a12 | gpmc_a12 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpmc_a0 | 5 | O | |||||||||||
| vin1b_fld1 | 6 | I | 0 | ||||||||||
| timer8 | 7 | IO | |||||||||||
| spi4_cs1 | 8 | IO | 1 | ||||||||||
| dma_evt1 | 9 | I | 0 | ||||||||||
| gpio2_2 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H3 | gpmc_a13 | gpmc_a13 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_rtclk | 1 | I | 0 | ||||||||||
| timer7 | 7 | IO | |||||||||||
| spi4_cs2 | 8 | IO | 1 | ||||||||||
| dma_evt2 | 9 | I | 0 | ||||||||||
| gpio2_3 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H4 | gpmc_a14 | gpmc_a14 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_d3 | 1 | IO | 0 | ||||||||||
| timer6 | 7 | IO | |||||||||||
| spi4_cs3 | 8 | IO | 1 | ||||||||||
| gpio2_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K6 | gpmc_a15 | gpmc_a15 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_d2 | 1 | IO | 0 | ||||||||||
| timer5 | 7 | IO | |||||||||||
| gpio2_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K5 | gpmc_a16 | gpmc_a16 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_d0 | 1 | IO | 0 | ||||||||||
| gpio2_6 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G2 | gpmc_a17 | gpmc_a17 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_d1 | 1 | IO | 0 | ||||||||||
| gpio2_7 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F2 | gpmc_a18 | gpmc_a18 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_sclk | 1 | IO | |||||||||||
| gpio2_8 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A4(9) | gpmc_a19 | gpmc_a19 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat4 | 1 | IO | 1 | ||||||||||
| gpmc_a13 | 2 | O | |||||||||||
| vin2b_d0 | 6 | I | 0 | ||||||||||
| gpio2_9 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E7(9) | gpmc_a20 | gpmc_a20 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat5 | 1 | IO | 1 | ||||||||||
| gpmc_a14 | 2 | O | |||||||||||
| vin2b_d1 | 6 | I | 0 | ||||||||||
| gpio2_10 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D6(9) | gpmc_a21 | gpmc_a21 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat6 | 1 | IO | 1 | ||||||||||
| gpmc_a15 | 2 | O | |||||||||||
| vin2b_d2 | 6 | I | 0 | ||||||||||
| gpio2_11 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C5(9) | gpmc_a22 | gpmc_a22 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat7 | 1 | IO | 1 | ||||||||||
| gpmc_a16 | 2 | O | |||||||||||
| vin2b_d3 | 6 | I | 0 | ||||||||||
| gpio2_12 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B5 | gpmc_a23 | gpmc_a23 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_clk | 1 | IO | 1 | ||||||||||
| gpmc_a17 | 2 | O | |||||||||||
| vin2b_d4 | 6 | I | 0 | ||||||||||
| gpio2_13 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D7(9) | gpmc_a24 | gpmc_a24 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat0 | 1 | IO | 1 | ||||||||||
| gpmc_a18 | 2 | O | |||||||||||
| vin2b_d5 | 6 | I | 0 | ||||||||||
| gpio2_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C6(9) | gpmc_a25 | gpmc_a25 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat1 | 1 | IO | 1 | ||||||||||
| gpmc_a19 | 2 | O | |||||||||||
| vin2b_d6 | 6 | I | 0 | ||||||||||
| gpio2_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A5(9) | gpmc_a26 | gpmc_a26 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat2 | 1 | IO | 1 | ||||||||||
| gpmc_a20 | 2 | O | |||||||||||
| vin2b_d7 | 6 | I | 0 | ||||||||||
| gpio2_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B6(9) | gpmc_a27 | gpmc_a27 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_dat3 | 1 | IO | 1 | ||||||||||
| gpmc_a21 | 2 | O | |||||||||||
| vin2b_hsync1 | 6 | I | |||||||||||
| gpio2_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F1 | gpmc_ad0 | gpmc_ad0 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d0 | 2 | I | 0 | ||||||||||
| vout3_d0 | 3 | O | |||||||||||
| gpio1_6 | 14 | IO | |||||||||||
| sysboot0 | 15 | I | |||||||||||
| E2 | gpmc_ad1 | gpmc_ad1 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d1 | 2 | I | 0 | ||||||||||
| vout3_d1 | 3 | O | |||||||||||
| gpio1_7 | 14 | IO | |||||||||||
| sysboot1 | 15 | I | |||||||||||
| E1 | gpmc_ad2 | gpmc_ad2 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d2 | 2 | I | 0 | ||||||||||
| vout3_d2 | 3 | O | |||||||||||
| gpio1_8 | 14 | IO | |||||||||||
| sysboot2 | 15 | I | |||||||||||
| C1 | gpmc_ad3 | gpmc_ad3 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d3 | 2 | I | 0 | ||||||||||
| vout3_d3 | 3 | O | |||||||||||
| gpio1_9 | 14 | IO | |||||||||||
| sysboot3 | 15 | I | |||||||||||
| D1 | gpmc_ad4 | gpmc_ad4 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d4 | 2 | I | 0 | ||||||||||
| vout3_d4 | 3 | O | |||||||||||
| gpio1_10 | 14 | IO | |||||||||||
| sysboot4 | 15 | I | |||||||||||
| D2 | gpmc_ad5 | gpmc_ad5 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d5 | 2 | I | 0 | ||||||||||
| vout3_d5 | 3 | O | |||||||||||
| gpio1_11 | 14 | IO | |||||||||||
| sysboot5 | 15 | I | |||||||||||
| B1 | gpmc_ad6 | gpmc_ad6 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d6 | 2 | I | 0 | ||||||||||
| vout3_d6 | 3 | O | |||||||||||
| gpio1_12 | 14 | IO | |||||||||||
| sysboot6 | 15 | I | |||||||||||
| B2 | gpmc_ad7 | gpmc_ad7 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d7 | 2 | I | 0 | ||||||||||
| vout3_d7 | 3 | O | |||||||||||
| gpio1_13 | 14 | IO | |||||||||||
| sysboot7 | 15 | I | |||||||||||
| C2 | gpmc_ad8 | gpmc_ad8 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d8 | 2 | I | 0 | ||||||||||
| vout3_d8 | 3 | O | |||||||||||
| gpio7_18 | 14 | IO | |||||||||||
| sysboot8 | 15 | I | |||||||||||
| D3 | gpmc_ad9 | gpmc_ad9 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d9 | 2 | I | 0 | ||||||||||
| vout3_d9 | 3 | O | |||||||||||
| gpio7_19 | 14 | IO | |||||||||||
| sysboot9 | 15 | I | |||||||||||
| A2 | gpmc_ad10 | gpmc_ad10 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d10 | 2 | I | 0 | ||||||||||
| vout3_d10 | 3 | O | |||||||||||
| gpio7_28 | 14 | IO | |||||||||||
| sysboot10 | 15 | I | |||||||||||
| B3 | gpmc_ad11 | gpmc_ad11 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d11 | 2 | I | 0 | ||||||||||
| vout3_d11 | 3 | O | |||||||||||
| gpio7_29 | 14 | IO | |||||||||||
| sysboot11 | 15 | I | |||||||||||
| C3 | gpmc_ad12 | gpmc_ad12 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d12 | 2 | I | 0 | ||||||||||
| vout3_d12 | 3 | O | |||||||||||
| gpio1_18 | 14 | IO | |||||||||||
| sysboot12 | 15 | I | |||||||||||
| C4 | gpmc_ad13 | gpmc_ad13 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d13 | 2 | I | 0 | ||||||||||
| vout3_d13 | 3 | O | |||||||||||
| gpio1_19 | 14 | IO | |||||||||||
| sysboot13 | 15 | I | |||||||||||
| A3 | gpmc_ad14 | gpmc_ad14 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d14 | 2 | I | 0 | ||||||||||
| vout3_d14 | 3 | O | |||||||||||
| gpio1_20 | 14 | IO | |||||||||||
| sysboot14 | 15 | I | |||||||||||
| B4 | gpmc_ad15 | gpmc_ad15 | 0 | IO | OFF | OFF | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d15 | 2 | I | 0 | ||||||||||
| vout3_d15 | 3 | O | |||||||||||
| gpio1_21 | 14 | IO | |||||||||||
| sysboot15 | 15 | I | |||||||||||
| H5 | gpmc_advn_ale | gpmc_advn_ale | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpmc_cs6 | 1 | O | |||||||||||
| clkout2 | 2 | O | |||||||||||
| gpmc_wait1 | 3 | I | 1 | ||||||||||
| gpmc_a2 | 5 | O | |||||||||||
| gpmc_a23 | 6 | O | |||||||||||
| timer3 | 7 | IO | |||||||||||
| i2c3_sda | 8 | IO | 1 | ||||||||||
| dma_evt2 | 9 | I | 0 | ||||||||||
| gpio2_23
gpmc_a19 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H2 | gpmc_ben0 | gpmc_ben0 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpmc_cs4 | 1 | O | |||||||||||
| vin2b_de1 | 6 | I | |||||||||||
| timer2 | 7 | IO | |||||||||||
| dma_evt3 | 9 | I | 0 | ||||||||||
| gpio2_26
gpmc_a21 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H6 | gpmc_ben1 | gpmc_ben1 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpmc_cs5 | 1 | O | |||||||||||
| vin2b_clk1 | 4 | I | |||||||||||
| gpmc_a3 | 5 | O | |||||||||||
| vin2b_fld1 | 6 | I | |||||||||||
| timer1 | 7 | IO | |||||||||||
| dma_evt4 | 9 | I | 0 | ||||||||||
| gpio2_27
gpmc_a22 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L4 | gpmc_clk | gpmc_clk | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| gpmc_cs7 | 1 | O | |||||||||||
| clkout1 | 2 | O | |||||||||||
| gpmc_wait1 | 3 | I | 1 | ||||||||||
| vin2b_clk1 | 6 | I | |||||||||||
| timer4 | 7 | IO | |||||||||||
| i2c3_scl | 8 | IO | 1 | ||||||||||
| dma_evt1 | 9 | I | 0 | ||||||||||
| gpio2_22
gpmc_a20 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F3 | gpmc_cs0 | gpmc_cs0 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio2_19 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A6 | gpmc_cs1 | gpmc_cs1 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv11 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc2_cmd | 1 | IO | 1 | ||||||||||
| gpmc_a22 | 2 | O | |||||||||||
| vin2b_vsync1 | 6 | I | |||||||||||
| gpio2_18 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G4 | gpmc_cs2 | gpmc_cs2 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_cs0 | 1 | IO | 1 | ||||||||||
| gpio2_20
gpmc_a23 gpmc_a13 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G3 | gpmc_cs3 | gpmc_cs3 | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| qspi1_cs1 | 1 | O | 1 | ||||||||||
| vin1a_clk0 | 2 | I | 0 | ||||||||||
| vout3_clk | 3 | O | |||||||||||
| gpmc_a1 | 5 | O | |||||||||||
| gpio2_21
gpmc_a24 gpmc_a14 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G5 | gpmc_oen_ren | gpmc_oen_ren | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio2_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F6 | gpmc_wait0 | gpmc_wait0 | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| gpio2_28
gpmc_a25 gpmc_a15 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G6 | gpmc_wen | gpmc_wen | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv10 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio2_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AE9 | hdmi1_clockx | hdmi1_clockx | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AD10 | hdmi1_clocky | hdmi1_clocky | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AE11 | hdmi1_data0x | hdmi1_data0x | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AD12 | hdmi1_data0y | hdmi1_data0y | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AE12 | hdmi1_data1x | hdmi1_data1x | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AD13 | hdmi1_data1y | hdmi1_data1y | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AE14 | hdmi1_data2x | hdmi1_data2x | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| AD15 | hdmi1_data2y | hdmi1_data2y | 0 | O | 1.8 | vdda_hdmi | HDMIPHY | Pdy | |||||
| G22 | i2c1_scl | i2c1_scl | 0 | IO | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS I2C | PU/PD | ||||
| Driver off | 15 | I | |||||||||||
| G23 | i2c1_sda | i2c1_sda | 0 | IO | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS I2C | PU/PD | ||||
| Driver off | 15 | I | |||||||||||
| G21 | i2c2_scl | i2c2_scl | 0 | IO | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS I2C | PU/PD | 1 | ||
| hdmi1_ddc_sda | 1 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F23 | i2c2_sda | i2c2_sda | 0 | IO | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS I2C | PU/PD | 1 | ||
| hdmi1_ddc_scl | 1 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AB9 | ljcb_clkn | ljcb_clkn | 0 | IO | 1.8 | vdda_pcie | LJCB | ||||||
| AC8 | ljcb_clkp | ljcb_clkp | 0 | IO | 1.8 | vdda_pcie | LJCB | ||||||
| D16 | mcasp1_aclkr | mcasp1_aclkr | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_axr2 | 1 | IO | 0 | ||||||||||
| i2c4_sda | 10 | IO | 1 | ||||||||||
| gpio5_0 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C16 | mcasp1_aclkx | mcasp1_aclkx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_fld0 | 7 | I | 0 | ||||||||||
| i2c3_sda | 10 | IO | 1 | ||||||||||
| gpio7_31 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D14 | mcasp1_axr0 | mcasp1_axr0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart6_rxd | 3 | I | 1 | ||||||||||
| vin1a_vsync0 | 7 | I | 0 | ||||||||||
| i2c5_sda | 10 | IO | 1 | ||||||||||
| gpio5_2 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B14 | mcasp1_axr1 | mcasp1_axr1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart6_txd | 3 | O | |||||||||||
| vin1a_hsync0 | 7 | I | 0 | ||||||||||
| i2c5_scl | 10 | IO | 1 | ||||||||||
| gpio5_3 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C14 | mcasp1_axr2 | mcasp1_axr2 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_axr2 | 1 | IO | 0 | ||||||||||
| uart6_ctsn | 3 | I | 1 | ||||||||||
| gpio5_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B15 | mcasp1_axr3 | mcasp1_axr3 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_axr3 | 1 | IO | 0 | ||||||||||
| uart6_rtsn | 3 | O | |||||||||||
| gpio5_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A15 | mcasp1_axr4 | mcasp1_axr4 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp4_axr2 | 1 | IO | 0 | ||||||||||
| gpio5_6 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A14 | mcasp1_axr5 | mcasp1_axr5 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp4_axr3 | 1 | IO | 0 | ||||||||||
| gpio5_7 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A17 | mcasp1_axr6 | mcasp1_axr6 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp5_axr2 | 1 | IO | 0 | ||||||||||
| gpio5_8 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A16 | mcasp1_axr7 | mcasp1_axr7 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp5_axr3 | 1 | IO | 0 | ||||||||||
| timer4 | 10 | IO | |||||||||||
| gpio5_9 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A18 | mcasp1_axr8 | mcasp1_axr8 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_axr0 | 1 | IO | 0 | ||||||||||
| spi3_sclk | 3 | IO | 0 | ||||||||||
| vin1a_d15 | 7 | I | 0 | ||||||||||
| timer5 | 10 | IO | |||||||||||
| gpio5_10 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B17 | mcasp1_axr9 | mcasp1_axr9 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_axr1 | 1 | IO | 0 | ||||||||||
| spi3_d1 | 3 | IO | 0 | ||||||||||
| vin1a_d14 | 7 | I | 0 | ||||||||||
| timer6 | 10 | IO | |||||||||||
| gpio5_11 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B16 | mcasp1_axr10 | mcasp1_axr10 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_aclkx | 1 | IO | 0 | ||||||||||
| mcasp6_aclkr | 2 | IO | |||||||||||
| spi3_d0 | 3 | IO | 0 | ||||||||||
| vin1a_d13 | 7 | I | 0 | ||||||||||
| timer7 | 10 | IO | |||||||||||
| gpio5_12 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B18 | mcasp1_axr11 | mcasp1_axr11 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp6_fsx | 1 | IO | 0 | ||||||||||
| mcasp6_fsr | 2 | IO | |||||||||||
| spi3_cs0 | 3 | IO | 1 | ||||||||||
| vin1a_d12 | 7 | I | 0 | ||||||||||
| timer8 | 10 | IO | |||||||||||
| gpio4_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A19 | mcasp1_axr12 | mcasp1_axr12 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_axr0 | 1 | IO | 0 | ||||||||||
| spi3_cs1 | 3 | IO | 1 | ||||||||||
| vin1a_d11 | 7 | I | 0 | ||||||||||
| timer9 | 10 | IO | |||||||||||
| gpio4_18 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E17 | mcasp1_axr13 | mcasp1_axr13 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_axr1 | 1 | IO | 0 | ||||||||||
| vin1a_d10 | 7 | I | 0 | ||||||||||
| timer10 | 10 | IO | |||||||||||
| gpio6_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E16 | mcasp1_axr14 | mcasp1_axr14 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_aclkx | 1 | IO | 0 | ||||||||||
| mcasp7_aclkr | 2 | IO | |||||||||||
| vin1a_d9 | 7 | I | 0 | ||||||||||
| timer11 | 10 | IO | |||||||||||
| gpio6_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F16 | mcasp1_axr15 | mcasp1_axr15 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_fsx | 1 | IO | 0 | ||||||||||
| mcasp7_fsr | 2 | IO | |||||||||||
| vin1a_d8 | 7 | I | 0 | ||||||||||
| timer12 | 10 | IO | |||||||||||
| gpio6_6 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D17 | mcasp1_fsr | mcasp1_fsr | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp7_axr3 | 1 | IO | 0 | ||||||||||
| i2c4_scl | 10 | IO | 1 | ||||||||||
| gpio5_1 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C17 | mcasp1_fsx | mcasp1_fsx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_de0 | 7 | I | 0 | ||||||||||
| i2c3_scl | 10 | IO | 1 | ||||||||||
| gpio7_30 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E19 | mcasp2_aclkx | mcasp2_aclkx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d7 | 7 | I | 0 | ||||||||||
| Driver off | 15 | I | |||||||||||
| A20 | mcasp2_axr0 | mcasp2_axr0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| Driver off | 15 | I | |||||||||||
| B19 | mcasp2_axr1 | mcasp2_axr1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| Driver off | 15 | I | |||||||||||
| A21 | mcasp2_axr2 | mcasp2_axr2 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp3_axr2 | 1 | IO | 0 | ||||||||||
| vin1a_d5 | 7 | I | 0 | ||||||||||
| gpio6_8 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B21 | mcasp2_axr3 | mcasp2_axr3 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp3_axr3 | 1 | IO | 0 | ||||||||||
| vin1a_d4 | 7 | I | 0 | ||||||||||
| gpio6_9 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B20 | mcasp2_axr4 | mcasp2_axr4 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp8_axr0 | 1 | IO | 0 | ||||||||||
| gpio1_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C19 | mcasp2_axr5 | mcasp2_axr5 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp8_axr1 | 1 | IO | 0 | ||||||||||
| gpio6_7 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D20 | mcasp2_axr6 | mcasp2_axr6 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp8_aclkx | 1 | IO | 0 | ||||||||||
| mcasp8_aclkr | 2 | IO | |||||||||||
| gpio2_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C20 | mcasp2_axr7 | mcasp2_axr7 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp8_fsx | 1 | IO | 0 | ||||||||||
| mcasp8_fsr | 2 | IO | |||||||||||
| gpio1_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D19 | mcasp2_fsx | mcasp2_fsx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin1a_d6 | 7 | I | 0 | ||||||||||
| Driver off | 15 | I | |||||||||||
| A22 | mcasp3_aclkx | mcasp3_aclkx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp3_aclkr | 1 | IO | |||||||||||
| mcasp2_axr12 | 2 | IO | 0 | ||||||||||
| uart7_rxd | 3 | I | 1 | ||||||||||
| vin1a_d3 | 7 | I | 0 | ||||||||||
| gpio5_13 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B22 | mcasp3_axr0 | mcasp3_axr0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp2_axr14 | 2 | IO | 0 | ||||||||||
| uart7_ctsn | 3 | I | 1 | ||||||||||
| uart5_rxd | 4 | I | 1 | ||||||||||
| vin1a_d1 | 7 | I | 0 | ||||||||||
| Driver off | 15 | I | |||||||||||
| B23 | mcasp3_axr1 | mcasp3_axr1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp2_axr15 | 2 | IO | 0 | ||||||||||
| uart7_rtsn | 3 | O | |||||||||||
| uart5_txd | 4 | O | |||||||||||
| vin1a_d0 | 7 | I | 0 | ||||||||||
| Driver off | 15 | I | |||||||||||
| A23 | mcasp3_fsx | mcasp3_fsx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp3_fsr | 1 | IO | |||||||||||
| mcasp2_axr13 | 2 | IO | 0 | ||||||||||
| uart7_txd | 3 | O | |||||||||||
| vin1a_d2 | 7 | I | 0 | ||||||||||
| gpio5_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C23 | mcasp4_aclkx | mcasp4_aclkx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp4_aclkr | 1 | IO | |||||||||||
| spi3_sclk | 2 | IO | 0 | ||||||||||
| uart8_rxd | 3 | I | 1 | ||||||||||
| i2c4_sda | 4 | IO | 1 | ||||||||||
| Driver off | 15 | I | |||||||||||
| A24 | mcasp4_axr0 | mcasp4_axr0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| spi3_d0 | 2 | IO | 0 | ||||||||||
| uart8_ctsn | 3 | I | 1 | ||||||||||
| uart4_rxd | 4 | I | 1 | ||||||||||
| i2c6_scl | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D23 | mcasp4_axr1 | mcasp4_axr1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| spi3_cs0 | 2 | IO | 1 | ||||||||||
| uart8_rtsn | 3 | O | |||||||||||
| uart4_txd | 4 | O | |||||||||||
| i2c6_sda | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B25 | mcasp4_fsx | mcasp4_fsx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp4_fsr | 1 | IO | |||||||||||
| spi3_d1 | 2 | IO | 0 | ||||||||||
| uart8_txd | 3 | O | |||||||||||
| i2c4_scl | 4 | IO | 1 | ||||||||||
| Driver off | 15 | I | |||||||||||
| AC3 | mcasp5_aclkx | mcasp5_aclkx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp5_aclkr | 1 | IO | |||||||||||
| spi4_sclk | 2 | IO | 0 | ||||||||||
| uart9_rxd | 3 | I | 1 | ||||||||||
| i2c5_sda | 4 | IO | 1 | ||||||||||
| Driver off | 15 | I | |||||||||||
| AA5 | mcasp5_axr0 | mcasp5_axr0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| spi4_d0 | 2 | IO | 0 | ||||||||||
| uart9_ctsn | 3 | I | 1 | ||||||||||
| uart3_rxd | 4 | I | 1 | ||||||||||
| Driver off | 15 | I | |||||||||||
| AC4 | mcasp5_axr1 | mcasp5_axr1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| spi4_cs0 | 2 | IO | 1 | ||||||||||
| uart9_rtsn | 3 | O | |||||||||||
| uart3_txd | 4 | O | |||||||||||
| Driver off | 15 | I | |||||||||||
| U6 | mcasp5_fsx | mcasp5_fsx | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mcasp5_fsr | 1 | IO | |||||||||||
| spi4_d1 | 2 | IO | 0 | ||||||||||
| uart9_txd | 3 | O | |||||||||||
| i2c5_scl | 4 | IO | 1 | ||||||||||
| Driver off | 15 | I | |||||||||||
| L6 | mdio_d | mdio_d | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart3_ctsn | 1 | I | 1 | ||||||||||
| mii0_txer | 3 | O | 0 | ||||||||||
| vin2a_d0 | 4 | I | 0 | ||||||||||
| vin1b_d0 | 5 | I | 0 | ||||||||||
| gpio5_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L5 | mdio_mclk | mdio_mclk | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart3_rtsn | 1 | O | |||||||||||
| mii0_col | 3 | I | 0 | ||||||||||
| vin2a_clk0 | 4 | I | |||||||||||
| vin1b_clk1 | 5 | I | 0 | ||||||||||
| gpio5_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| U3 | mmc1_clk | mmc1_clk | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_21 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| V4 | mmc1_cmd | mmc1_cmd | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_22 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| V3 | mmc1_dat0 | mmc1_dat0 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_23 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| V2 | mmc1_dat1 | mmc1_dat1 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| W1 | mmc1_dat2 | mmc1_dat2 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| V1 | mmc1_dat3 | mmc1_dat3 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | SDIO2KV1833 | Pux/PDy | 1 |
| gpio6_26 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| U5 | mmc1_sdcd | mmc1_sdcd | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv8 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart6_rxd | 3 | I | 1 | ||||||||||
| i2c4_sda | 4 | IO | 1 | ||||||||||
| gpio6_27 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| V5 | mmc1_sdwp | mmc1_sdwp | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv8 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart6_txd | 3 | O | |||||||||||
| i2c4_scl | 4 | IO | 1 | ||||||||||
| gpio6_28 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y2 | mmc3_clk | mmc3_clk | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| usb3_ulpi_d5 | 3 | IO | 0 | ||||||||||
| vin2b_d7 | 4 | I | 0 | ||||||||||
| vin1a_d7 | 9 | I | 0 | ||||||||||
| ehrpwm2_tripzone_input | 10 | IO | 0 | ||||||||||
| gpio6_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y1 | mmc3_cmd | mmc3_cmd | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi3_sclk | 1 | IO | 0 | ||||||||||
| usb3_ulpi_d4 | 3 | IO | 0 | ||||||||||
| vin2b_d6 | 4 | I | 0 | ||||||||||
| vin1a_d6 | 9 | I | 0 | ||||||||||
| eCAP2_in_PWM2_out | 10 | IO | 0 | ||||||||||
| gpio6_30 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y4 | mmc3_dat0 | mmc3_dat0 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi3_d1 | 1 | IO | 0 | ||||||||||
| uart5_rxd | 2 | I | 1 | ||||||||||
| usb3_ulpi_d3 | 3 | IO | 0 | ||||||||||
| vin2b_d5 | 4 | I | 0 | ||||||||||
| vin1a_d5 | 9 | I | 0 | ||||||||||
| eQEP3A_in | 10 | I | 0 | ||||||||||
| gpio6_31 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AA2 | mmc3_dat1 | mmc3_dat1 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi3_d0 | 1 | IO | 0 | ||||||||||
| uart5_txd | 2 | O | |||||||||||
| usb3_ulpi_d2 | 3 | IO | 0 | ||||||||||
| vin2b_d4 | 4 | I | 0 | ||||||||||
| vin1a_d4 | 9 | I | 0 | ||||||||||
| eQEP3B_in | 10 | I | 0 | ||||||||||
| gpio7_0 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AA3 | mmc3_dat2 | mmc3_dat2 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi3_cs0 | 1 | IO | 1 | ||||||||||
| uart5_ctsn | 2 | I | 1 | ||||||||||
| usb3_ulpi_d1 | 3 | IO | 0 | ||||||||||
| vin2b_d3 | 4 | I | 0 | ||||||||||
| vin1a_d3 | 9 | I | 0 | ||||||||||
| eQEP3_index | 10 | IO | 0 | ||||||||||
| gpio7_1 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| W2 | mmc3_dat3 | mmc3_dat3 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi3_cs1 | 1 | IO | 1 | ||||||||||
| uart5_rtsn | 2 | O | |||||||||||
| usb3_ulpi_d0 | 3 | IO | 0 | ||||||||||
| vin2b_d2 | 4 | I | 0 | ||||||||||
| vin1a_d2 | 9 | I | 0 | ||||||||||
| eQEP3_strobe | 10 | IO | 0 | ||||||||||
| gpio7_2 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y3 | mmc3_dat4 | mmc3_dat4 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi4_sclk | 1 | IO | 0 | ||||||||||
| uart10_rxd | 2 | I | 1 | ||||||||||
| usb3_ulpi_nxt | 3 | I | 0 | ||||||||||
| vin2b_d1 | 4 | I | 0 | ||||||||||
| vin1a_d1 | 9 | I | 0 | ||||||||||
| ehrpwm3A | 10 | O | |||||||||||
| gpio1_22 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AA1 | mmc3_dat5 | mmc3_dat5 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi4_d1 | 1 | IO | 0 | ||||||||||
| uart10_txd | 2 | O | |||||||||||
| usb3_ulpi_dir | 3 | I | 0 | ||||||||||
| vin2b_d0 | 4 | I | 0 | ||||||||||
| vin1a_d0 | 9 | I | 0 | ||||||||||
| ehrpwm3B | 10 | O | |||||||||||
| gpio1_23 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AA4 | mmc3_dat6 | mmc3_dat6 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi4_d0 | 1 | IO | 0 | ||||||||||
| uart10_ctsn | 2 | I | 1 | ||||||||||
| usb3_ulpi_stp | 3 | O | |||||||||||
| vin2b_de1 | 4 | I | |||||||||||
| vin1a_hsync0 | 9 | I | 0 | ||||||||||
| ehrpwm3_tripzone_input | 10 | IO | 0 | ||||||||||
| gpio1_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AB1 | mmc3_dat7 | mmc3_dat7 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv7 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi4_cs0 | 1 | IO | 1 | ||||||||||
| uart10_rtsn | 2 | O | |||||||||||
| usb3_ulpi_clk | 3 | I | 0 | ||||||||||
| vin2b_clk1 | 4 | I | |||||||||||
| vin1a_vsync0 | 9 | I | 0 | ||||||||||
| eCAP3_in_PWM3_out | 10 | IO | 0 | ||||||||||
| gpio1_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L24 | nmin_dsp | nmin_dsp | 0 | I | PD | PD | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | ||
| AE6 | pcie_rxn0 | pcie_rxn0 | 0 | I | OFF | OFF | 1.8 | vdda_pcie | SERDES | ||||
| AD7 | pcie_rxp0 | pcie_rxp0 | 0 | I | OFF | OFF | 1.8 | vdda_pcie | SERDES | ||||
| AE8 | pcie_txn0 | pcie_txn0 | 0 | O | 1.8 | vdda_pcie | SERDES | ||||||
| AD9 | pcie_txp0 | pcie_txp0 | 0 | O | 1.8 | vdda_pcie | SERDES | ||||||
| F19 | porz | porz | 0 | I | 1.8/3.3 | vddshv3 | Yes | IHHV1833 | PU/PD | ||||
| K24 | resetn | resetn | 0 | I | PU | PU | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | ||
| N2 | rgmii0_rxc | rgmii0_rxc | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii1_txen | 2 | O | |||||||||||
| mii0_txclk | 3 | I | 0 | ||||||||||
| vin2a_d5 | 4 | I | 0 | ||||||||||
| vin1b_d5 | 5 | I | 0 | ||||||||||
| usb3_ulpi_d2 | 6 | IO | 0 | ||||||||||
| gpio5_26 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| P2 | rgmii0_rxctl | rgmii0_rxctl | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii1_txd1 | 2 | O | |||||||||||
| mii0_txd3 | 3 | O | |||||||||||
| vin2a_d6 | 4 | I | 0 | ||||||||||
| vin1b_d6 | 5 | I | 0 | ||||||||||
| usb3_ulpi_d3 | 6 | IO | 0 | ||||||||||
| gpio5_27 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N4 | rgmii0_rxd0 | rgmii0_rxd0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii0_txd0 | 1 | O | |||||||||||
| mii0_txd0 | 3 | O | |||||||||||
| vin2a_fld0 | 4 | I | |||||||||||
| vin1b_fld1 | 5 | I | 0 | ||||||||||
| usb3_ulpi_d7 | 6 | IO | 0 | ||||||||||
| gpio5_31 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N3 | rgmii0_rxd1 | rgmii0_rxd1 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii0_txd1 | 1 | O | |||||||||||
| mii0_txd1 | 3 | O | |||||||||||
| vin2a_d9 | 4 | I | 0 | ||||||||||
| usb3_ulpi_d6 | 6 | IO | 0 | ||||||||||
| gpio5_30 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| P1 | rgmii0_rxd2 | rgmii0_rxd2 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii0_txen | 1 | O | |||||||||||
| mii0_txen | 3 | O | |||||||||||
| vin2a_d8 | 4 | I | 0 | ||||||||||
| usb3_ulpi_d5 | 6 | IO | 0 | ||||||||||
| gpio5_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N1 | rgmii0_rxd3 | rgmii0_rxd3 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rmii1_txd0 | 2 | O | |||||||||||
| mii0_txd2 | 3 | O | |||||||||||
| vin2a_d7 | 4 | I | 0 | ||||||||||
| vin1b_d7 | 5 | I | 0 | ||||||||||
| usb3_ulpi_d4 | 6 | IO | 0 | ||||||||||
| gpio5_28 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| T4 | rgmii0_txc | rgmii0_txc | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| uart3_ctsn | 1 | I | 1 | ||||||||||
| rmii1_rxd1 | 2 | I | 0 | ||||||||||
| mii0_rxd3 | 3 | I | 0 | ||||||||||
| vin2a_d3 | 4 | I | 0 | ||||||||||
| vin1b_d3 | 5 | I | 0 | ||||||||||
| usb3_ulpi_clk | 6 | I | 0 | ||||||||||
| spi3_d0 | 7 | IO | 0 | ||||||||||
| spi4_cs2 | 8 | IO | 1 | ||||||||||
| gpio5_20 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| T5 | rgmii0_txctl | rgmii0_txctl | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| uart3_rtsn | 1 | O | |||||||||||
| rmii1_rxd0 | 2 | I | 0 | ||||||||||
| mii0_rxd2 | 3 | I | 0 | ||||||||||
| vin2a_d4 | 4 | I | 0 | ||||||||||
| vin1b_d4 | 5 | I | 0 | ||||||||||
| usb3_ulpi_stp | 6 | O | |||||||||||
| spi3_cs0 | 7 | IO | 1 | ||||||||||
| spi4_cs3 | 8 | IO | 1 | ||||||||||
| gpio5_21 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| R1 | rgmii0_txd0 | rgmii0_txd0 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| rmii0_rxd0 | 1 | I | 0 | ||||||||||
| mii0_rxd0 | 3 | I | 0 | ||||||||||
| vin2a_d10 | 4 | I | 0 | ||||||||||
| usb3_ulpi_d1 | 6 | IO | 0 | ||||||||||
| spi4_cs0 | 7 | IO | 1 | ||||||||||
| uart4_rtsn | 8 | O | |||||||||||
| gpio5_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| R2 | rgmii0_txd1 | rgmii0_txd1 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| rmii0_rxd1 | 1 | I | 0 | ||||||||||
| mii0_rxd1 | 3 | I | 0 | ||||||||||
| vin2a_vsync0 | 4 | I | |||||||||||
| vin1b_vsync1 | 5 | I | 0 | ||||||||||
| usb3_ulpi_d0 | 6 | IO | 0 | ||||||||||
| spi4_d0 | 7 | IO | 0 | ||||||||||
| uart4_ctsn | 8 | IO | 1 | ||||||||||
| gpio5_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| P3 | rgmii0_txd2 | rgmii0_txd2 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| rmii0_rxer | 1 | I | 0 | ||||||||||
| mii0_rxer | 3 | I | 0 | ||||||||||
| vin2a_hsync0 | 4 | I | |||||||||||
| vin1b_hsync1 | 5 | I | 0 | ||||||||||
| usb3_ulpi_nxt | 6 | I | 0 | ||||||||||
| spi4_d1 | 7 | IO | 0 | ||||||||||
| uart4_txd | 8 | O | |||||||||||
| gpio5_23 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| P4 | rgmii0_txd3 | rgmii0_txd3 | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| rmii0_crs | 1 | I | 0 | ||||||||||
| mii0_crs | 3 | I | 0 | ||||||||||
| vin2a_de0 | 4 | I | |||||||||||
| vin1b_de1 | 5 | I | 0 | ||||||||||
| usb3_ulpi_dir | 6 | I | 0 | ||||||||||
| spi4_sclk | 7 | IO | 0 | ||||||||||
| uart4_rxd | 8 | I | 1 | ||||||||||
| gpio5_22 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| P5 | RMII_MHZ_50_CLK | RMII_MHZ_50_CLK | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2a_d11 | 4 | I | 0 | ||||||||||
| gpio5_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E20 | rstoutn | rstoutn | 0 | O | PD | PD | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | ||
| K25 | rtck | rtck | 0 | O | PU | OFF | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio8_29 | 14 | IO | |||||||||||
| B24 | spi1_cs0 | spi1_cs0 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| gpio7_10 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C25 | spi1_cs1 | spi1_cs1 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| spi2_cs1 | 3 | IO | 1 | ||||||||||
| gpio7_11 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E24 | spi1_cs2 | spi1_cs2 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart4_rxd | 1 | I | 1 | ||||||||||
| mmc3_sdcd | 2 | I | 1 | ||||||||||
| spi2_cs2 | 3 | IO | 1 | ||||||||||
| dcan2_tx | 4 | IO | 1 | ||||||||||
| mdio_mclk | 5 | O | 1 | ||||||||||
| hdmi1_hpd | 6 | IO | |||||||||||
| gpio7_12 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E25 | spi1_cs3 | spi1_cs3 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart4_txd | 1 | O | |||||||||||
| mmc3_sdwp | 2 | I | 0 | ||||||||||
| spi2_cs3 | 3 | IO | 1 | ||||||||||
| dcan2_rx | 4 | IO | 1 | ||||||||||
| mdio_d | 5 | IO | 1 | ||||||||||
| hdmi1_cec | 6 | IO | |||||||||||
| gpio7_13 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D25 | spi1_d0 | spi1_d0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| gpio7_9 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D24 | spi1_d1 | spi1_d1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| gpio7_8 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C24 | spi1_sclk | spi1_sclk | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| gpio7_7 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F24 | spi2_cs0 | spi2_cs0 | 0 | IO | PU | PU | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart3_rtsn | 1 | O | |||||||||||
| uart5_txd | 2 | O | |||||||||||
| gpio7_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G24 | spi2_d0 | spi2_d0 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart3_ctsn | 1 | I | 1 | ||||||||||
| uart5_rxd | 2 | I | 1 | ||||||||||
| gpio7_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F25 | spi2_d1 | spi2_d1 | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart3_txd | 1 | O | |||||||||||
| gpio7_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| G25 | spi2_sclk | spi2_sclk | 0 | IO | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| uart3_rxd | 1 | I | 1 | ||||||||||
| gpio7_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| K21 | tclk | tclk | 0 | I | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | IQ1833 | PU/PD | |
| L23 | tdi | tdi | 0 | I | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio8_27 | 14 | I | |||||||||||
| J20 | tdo | tdo | 0 | O | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| gpio8_28 | 14 | IO | |||||||||||
| L21 | tms | tms | 0 | I | PU | PU | 0 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| L22 | trstn | trstn | 0 | I | PD | PD | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | ||
| L20 | uart1_ctsn | uart1_ctsn | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart9_rxd | 2 | I | 1 | ||||||||||
| mmc4_clk | 3 | IO | 1 | ||||||||||
| gpio7_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| M24 | uart1_rtsn | uart1_rtsn | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | |
| uart9_txd | 2 | O | |||||||||||
| mmc4_cmd | 3 | IO | 1 | ||||||||||
| gpio7_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| L25 | uart1_rxd | uart1_rxd | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| mmc4_sdcd | 3 | I | 1 | ||||||||||
| gpio7_22 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| M25 | uart1_txd | uart1_txd | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mmc4_sdwp | 3 | I | 0 | ||||||||||
| gpio7_23 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N22 | uart2_ctsn | uart2_ctsn | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart3_rxd | 2 | I | 1 | ||||||||||
| mmc4_dat2 | 3 | IO | 1 | ||||||||||
| uart10_rxd | 4 | I | 1 | ||||||||||
| uart1_dtrn | 5 | O | |||||||||||
| gpio1_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N24 | uart2_rtsn | uart2_rtsn | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | |
| uart3_txd | 1 | O | |||||||||||
| uart3_irtx | 2 | O | |||||||||||
| mmc4_dat3 | 3 | IO | 1 | ||||||||||
| uart10_txd | 4 | O | |||||||||||
| uart1_rin | 5 | I | 1 | ||||||||||
| gpio1_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N23 | uart2_rxd | uart2_rxd | 0 | I | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| uart3_ctsn | 1 | I | 1 | ||||||||||
| uart3_rctx | 2 | O | |||||||||||
| mmc4_dat0 | 3 | IO | 1 | ||||||||||
| uart2_rxd | 4 | I | 1 | ||||||||||
| uart1_dcdn | 5 | I | 1 | ||||||||||
| gpio7_26 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N25 | uart2_txd | uart2_txd | 0 | O | PU | PU | 15 | 1.8/3.3 | vddshv4 | Yes | Dual Voltage LVCMOS | PU/PD | |
| uart3_rtsn | 1 | O | |||||||||||
| uart3_sd | 2 | O | |||||||||||
| mmc4_dat1 | 3 | IO | 1 | ||||||||||
| uart2_txd | 4 | O | |||||||||||
| uart1_dsrn | 5 | I | 0 | ||||||||||
| gpio7_27 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N5 | uart3_rxd | uart3_rxd | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | 1 |
| rmii1_crs | 2 | I | 0 | ||||||||||
| mii0_rxdv | 3 | I | 0 | ||||||||||
| vin2a_d1 | 4 | I | 0 | ||||||||||
| vin1b_d1 | 5 | I | 0 | ||||||||||
| spi3_sclk | 7 | IO | 0 | ||||||||||
| gpio5_18 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| N6 | uart3_txd | uart3_txd | 0 | O | PD | PD | 15 | 1.8/3.3 | vddshv9 | Yes | Dual Voltage LVCMOS | PU/PD | |
| rmii1_rxer | 2 | I | 0 | ||||||||||
| mii0_rxclk | 3 | I | 0 | ||||||||||
| vin2a_d2 | 4 | I | 0 | ||||||||||
| vin1b_d2 | 5 | I | 0 | ||||||||||
| spi3_d1 | 7 | IO | 0 | ||||||||||
| spi4_cs1 | 8 | IO | 1 | ||||||||||
| gpio5_19 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AB7 | usb1_dm | usb1_dm | 0 | IO | OFF | OFF | 3.3 | vdda33v_usb1 | USBPHY | ||||
| AC6 | usb1_dp | usb1_dp | 0 | IO | OFF | OFF | 3.3 | vdda33v_usb1 | USBPHY | ||||
| AD3 | usb1_drvvbus | usb1_drvvbus | 0 | O | PD | PD | 15 | 1.8/3.3 | vdda33v_usb2 | Yes | Dual Voltage LVCMOS | PU/PD | |
| timer16 | 7 | IO | |||||||||||
| gpio6_12 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AC5 | usb2_dm | usb2_dm | 0 | IO | 3.3 | vdda33v_usb2 | No | USBPHY | |||||
| AB6 | usb2_dp | usb2_dp | 0 | IO | 3.3 | vdda33v_usb2 | No | USBPHY | |||||
| AA6 | usb2_drvvbus | usb2_drvvbus | 0 | O | PD | PD | 15 | 1.8/3.3 | vdda33v_usb2 | Yes | Dual Voltage LVCMOS | PU/PD | |
| timer15 | 7 | IO | |||||||||||
| gpio6_13 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| AE5 | usb_rxn0 | usb_rxn0 | 0 | I | OFF | OFF | 1.8 | vdda_usb1 | SERDES | ||||
| pcie_rxn1 | 1 | I | |||||||||||
| AD6 | usb_rxp0 | usb_rxp0 | 0 | I | OFF | OFF | 1.8 | vdda_usb1 | SERDES | ||||
| pcie_rxp1 | 1 | I | |||||||||||
| AE3 | usb_txn0 | usb_txn0 | 0 | O | 1.8 | vdda_usb1 | SERDES | ||||||
| pcie_txn1 | 1 | O | |||||||||||
| AD4 | usb_txp0 | usb_txp0 | 0 | O | 1.8 | vdda_usb1 | SERDES | ||||||
| pcie_txp1 | 1 | O | |||||||||||
| J15, J16, J18, K12, K18, L12, L17, M11, M13, M15, M17, N11, N13, N15, N18, P10, P12, P14, P16, P18, R10, R12, R14, R16, R17, T11, T13, T15, T17, T9, U11, U13, U15, U18, U9, V10, V12, V14, V16, V18, W10, W12, W14, W16 | vdd | vdd | PWR | ||||||||||
| F20 | vpp | vpp(10) | PWR | ||||||||||
| AA10 | vdda33v_usb1 | vdda33v_usb1 | PWR | ||||||||||
| Y10 | vdda33v_usb2 | vdda33v_usb2 | PWR | ||||||||||
| L9 | vdda_core_gmac | vdda_core_gmac | PWR | ||||||||||
| T6 | vdda_csi | vdda_csi | PWR | ||||||||||
| R20 | vdda_ddr | vdda_ddr | PWR | ||||||||||
| N10 | vdda_debug | vdda_debug | PWR | ||||||||||
| K10, L10 | vdda_dsp_iva | vdda_dsp_iva | PWR | ||||||||||
| N9 | vdda_gpu | vdda_gpu | PWR | ||||||||||
| W15, Y15 | vdda_hdmi | vdda_hdmi | PWR | ||||||||||
| K16, L16 | vdda_mpu_abe | vdda_mpu_abe | PWR | ||||||||||
| W13, Y13 | vdda_osc | vdda_osc | PWR | ||||||||||
| W11, Y11 | vdda_pcie | vdda_pcie | PWR | ||||||||||
| M10 | vdda_per | vdda_per | PWR | ||||||||||
| W8 | vdda_usb1 | vdda_usb1 | PWR | ||||||||||
| Y8 | vdda_usb2 | vdda_usb2 | PWR | ||||||||||
| Y9 | vdda_usb3 | vdda_usb3 | PWR | ||||||||||
| K14, L14 | vdda_video | vdda_video | PWR | ||||||||||
| G11, H20, W7, Y18 | vdds18v | vdds18v | PWR | ||||||||||
| AA19, P20, Y19 | vdds18v_ddr1 | vdds18v_ddr1 | PWR | ||||||||||
| G10, G9 | vddshv1 | vddshv1 | PWR | ||||||||||
| G15, G17, H15, H17, J19, K19 | vddshv3 | vddshv3 | PWR | ||||||||||
| M19, N19 | vddshv4 | vddshv4 | PWR | ||||||||||
| U7, U8 | vddshv7 | vddshv7 | PWR | ||||||||||
| N8, P8 | vddshv8 | vddshv8 | PWR | ||||||||||
| M7, N7 | vddshv9 | vddshv9 | PWR | ||||||||||
| J7, J8, K8 | vddshv10 | vddshv10 | PWR | ||||||||||
| F7, G7, H7 | vddshv11 | vddshv11 | PWR | ||||||||||
| T19, T20, V20, W17, W18, W20 | vdds_ddr1 | vdds_ddr1 | PWR | ||||||||||
| P7, R7 | vdds_mlbp | vdds_mlbp | PWR | ||||||||||
| H11, H13, H9, J11, J13, J9 | vdd_dsp | vdd_dsp | PWR | ||||||||||
| D8 | vin2a_clk0 | vin2a_clk0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vout2_fld | 4 | O | |||||||||||
| emu5 | 5 | O | |||||||||||
| eQEP1A_in | 10 | I | 0 | ||||||||||
| gpio3_28
gpmc_a27 gpmc_a17 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C8 | vin2a_d0 | vin2a_d0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d23 | 4 | O | |||||||||||
| emu10 | 5 | O | |||||||||||
| uart9_ctsn | 7 | I | 1 | ||||||||||
| spi4_d0 | 8 | IO | 0 | ||||||||||
| ehrpwm1B | 10 | O | |||||||||||
| gpio4_1 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B9 | vin2a_d1 | vin2a_d1 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d22 | 4 | O | |||||||||||
| emu11 | 5 | O | |||||||||||
| uart9_rtsn | 7 | O | |||||||||||
| spi4_cs0 | 8 | IO | 1 | ||||||||||
| ehrpwm1_tripzone_input | 10 | IO | 0 | ||||||||||
| gpio4_2 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A7 | vin2a_d2 | vin2a_d2 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d21 | 4 | O | |||||||||||
| emu12 | 5 | O | |||||||||||
| uart10_rxd | 8 | I | 1 | ||||||||||
| eCAP1_in_PWM1_out | 10 | IO | 0 | ||||||||||
| gpio4_3 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A9 | vin2a_d3 | vin2a_d3 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d20 | 4 | O | |||||||||||
| emu13 | 5 | O | |||||||||||
| uart10_txd | 8 | O | |||||||||||
| ehrpwm1_synci | 10 | I | 0 | ||||||||||
| gpio4_4 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A8 | vin2a_d4 | vin2a_d4 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d19 | 4 | O | |||||||||||
| emu14 | 5 | O | |||||||||||
| uart10_ctsn | 8 | I | 1 | ||||||||||
| ehrpwm1_synco | 10 | O | |||||||||||
| gpio4_5 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A11 | vin2a_d5 | vin2a_d5 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d18 | 4 | O | |||||||||||
| emu15 | 5 | O | |||||||||||
| uart10_rtsn | 8 | O | |||||||||||
| eQEP2A_in | 10 | I | 0 | ||||||||||
| gpio4_6 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F10 | vin2a_d6 | vin2a_d6 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d17 | 4 | O | |||||||||||
| emu16 | 5 | O | |||||||||||
| mii1_rxd1 | 8 | I | 0 | ||||||||||
| eQEP2B_in | 10 | I | 0 | ||||||||||
| gpio4_7 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A10 | vin2a_d7 | vin2a_d7 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d16 | 4 | O | |||||||||||
| emu17 | 5 | O | |||||||||||
| mii1_rxd2 | 8 | I | 0 | ||||||||||
| eQEP2_index | 10 | IO | 0 | ||||||||||
| gpio4_8 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B10 | vin2a_d8 | vin2a_d8 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d15 | 4 | O | |||||||||||
| emu18 | 5 | O | |||||||||||
| mii1_rxd3 | 8 | I | 0 | ||||||||||
| eQEP2_strobe | 10 | IO | 0 | ||||||||||
| gpio4_9
gpmc_a26 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E10 | vin2a_d9 | vin2a_d9 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vout2_d14 | 4 | O | |||||||||||
| emu19 | 5 | O | |||||||||||
| mii1_rxd0 | 8 | I | 0 | ||||||||||
| ehrpwm2A | 10 | O | |||||||||||
| gpio4_10
gpmc_a25 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D10 | vin2a_d10 | vin2a_d10 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mdio_mclk | 3 | O | 1 | ||||||||||
| vout2_d13 | 4 | O | |||||||||||
| ehrpwm2B | 10 | O | |||||||||||
| gpio4_11
gpmc_a24 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C10 | vin2a_d11 | vin2a_d11 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| mdio_d | 3 | IO | 1 | ||||||||||
| vout2_d12 | 4 | O | |||||||||||
| ehrpwm2_tripzone_input | 10 | IO | 0 | ||||||||||
| gpio4_12
gpmc_a23 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B11 | vin2a_d12 | vin2a_d12 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rgmii1_txc | 3 | O | |||||||||||
| vout2_d11 | 4 | O | |||||||||||
| mii1_rxclk | 8 | I | 0 | ||||||||||
| eCAP2_in_PWM2_out | 10 | IO | 0 | ||||||||||
| gpio4_13 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D11 | vin2a_d13 | vin2a_d13 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rgmii1_txctl | 3 | O | |||||||||||
| vout2_d10 | 4 | O | |||||||||||
| mii1_rxdv | 8 | I | 0 | ||||||||||
| eQEP3A_in | 10 | I | 0 | ||||||||||
| gpio4_14 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C11 | vin2a_d14 | vin2a_d14 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rgmii1_txd3 | 3 | O | |||||||||||
| vout2_d9 | 4 | O | |||||||||||
| mii1_txclk | 8 | I | 0 | ||||||||||
| eQEP3B_in | 10 | I | 0 | ||||||||||
| gpio4_15 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B12 | vin2a_d15 | vin2a_d15 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| rgmii1_txd2 | 3 | O | |||||||||||
| vout2_d8 | 4 | O | |||||||||||
| mii1_txd0 | 8 | O | |||||||||||
| eQEP3_index | 10 | IO | 0 | ||||||||||
| gpio4_16 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A12 | vin2a_d16 | vin2a_d16 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d7 | 2 | I | 0 | ||||||||||
| rgmii1_txd1 | 3 | O | |||||||||||
| vout2_d7 | 4 | O | |||||||||||
| mii1_txd1 | 8 | O | |||||||||||
| eQEP3_strobe | 10 | IO | 0 | ||||||||||
| gpio4_24 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A13 | vin2a_d17 | vin2a_d17 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d6 | 2 | I | 0 | ||||||||||
| rgmii1_txd0 | 3 | O | |||||||||||
| vout2_d6 | 4 | O | |||||||||||
| mii1_txd2 | 8 | O | |||||||||||
| ehrpwm3A | 10 | O | |||||||||||
| gpio4_25 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E11 | vin2a_d18 | vin2a_d18 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d5 | 2 | I | 0 | ||||||||||
| rgmii1_rxc | 3 | I | 0 | ||||||||||
| vout2_d5 | 4 | O | |||||||||||
| mii1_txd3 | 8 | O | |||||||||||
| ehrpwm3B | 10 | O | |||||||||||
| gpio4_26 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| F11 | vin2a_d19 | vin2a_d19 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d4 | 2 | I | 0 | ||||||||||
| rgmii1_rxctl | 3 | I | 0 | ||||||||||
| vout2_d4 | 4 | O | |||||||||||
| mii1_txer | 8 | O | 0 | ||||||||||
| ehrpwm3_tripzone_input | 10 | IO | 0 | ||||||||||
| gpio4_27 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B13 | vin2a_d20 | vin2a_d20 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d3 | 2 | I | 0 | ||||||||||
| rgmii1_rxd3 | 3 | I | 0 | ||||||||||
| vout2_d3 | 4 | O | |||||||||||
| mii1_rxer | 8 | I | 0 | ||||||||||
| eCAP3_in_PWM3_out | 10 | IO | 0 | ||||||||||
| gpio4_28 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E13 | vin2a_d21 | vin2a_d21 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d2 | 2 | I | 0 | ||||||||||
| rgmii1_rxd2 | 3 | I | 0 | ||||||||||
| vout2_d2 | 4 | O | |||||||||||
| mii1_col | 8 | I | 0 | ||||||||||
| gpio4_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C13 | vin2a_d22 | vin2a_d22 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d1 | 2 | I | 0 | ||||||||||
| rgmii1_rxd1 | 3 | I | 0 | ||||||||||
| vout2_d1 | 4 | O | |||||||||||
| mii1_crs | 8 | I | 0 | ||||||||||
| gpio4_30 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| D13 | vin2a_d23 | vin2a_d23 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | 0 |
| vin2b_d0 | 2 | I | 0 | ||||||||||
| rgmii1_rxd0 | 3 | I | 0 | ||||||||||
| vout2_d0 | 4 | O | |||||||||||
| mii1_txen | 8 | O | |||||||||||
| gpio4_31 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B7 | vin2a_de0 | vin2a_de0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin2a_fld0 | 1 | I | |||||||||||
| vin2b_fld1 | 2 | I | |||||||||||
| vin2b_de1 | 3 | I | |||||||||||
| vout2_de | 4 | O | |||||||||||
| emu6 | 5 | O | |||||||||||
| eQEP1B_in | 10 | I | 0 | ||||||||||
| gpio3_29 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| C7 | vin2a_fld0 | vin2a_fld0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin2b_clk1 | 2 | I | |||||||||||
| vout2_clk | 4 | O | |||||||||||
| emu7 | 5 | O | |||||||||||
| eQEP1_index | 10 | IO | 0 | ||||||||||
| gpio3_30
gpmc_a27 gpmc_a18 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| E8 | vin2a_hsync0 | vin2a_hsync0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin2b_hsync1 | 3 | I | |||||||||||
| vout2_hsync | 4 | O | |||||||||||
| emu8 | 5 | O | |||||||||||
| uart9_rxd | 7 | I | 1 | ||||||||||
| spi4_sclk | 8 | IO | 0 | ||||||||||
| eQEP1_strobe | 10 | IO | 0 | ||||||||||
| gpio3_31
gpmc_a27 |
14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| B8 | vin2a_vsync0 | vin2a_vsync0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv1 | Yes | Dual Voltage LVCMOS | PU/PD | |
| vin2b_vsync1 | 3 | I | |||||||||||
| vout2_vsync | 4 | O | |||||||||||
| emu9 | 5 | O | |||||||||||
| uart9_txd | 7 | O | |||||||||||
| spi4_d1 | 8 | IO | 0 | ||||||||||
| ehrpwm1A | 10 | O | |||||||||||
| gpio4_0 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| A1, A25, AA13, AA15, AA7, AA8, AA9, AB8, AC13, AE1, AE15, AE25, G13, G16, G8, H10, H12, H14, H16, H18, H19, H8, J10, J12, J14, J17, K11, K13, K15, K17, K9, L11, L13, L15, L18, L8, M12, M14, M16, M18, M20, M8, M9, N12, N14, N16, N17, N20, P11, P13, P15, P17, P19, P9, R11, R13, R15, R18, R19, R8, R9, T10, T12, T14, T16, T18, T8, U10, U12, U14, U16, U17, U19, V11, V13, V15, V17, V19, V8, V9, W19, W9, Y14, Y16, Y17, Y7 | vss | vss | GND | ||||||||||
| AA12 | vssa_osc0 | vssa_osc0 | GND | ||||||||||
| AB11 | vssa_osc1 | vssa_osc1 | GND | ||||||||||
| AC10 | Wakeup0 | dcan1_rx | 1 | I | 15 | 1.8/3.3 | vdda33v_usb1 | Yes | IHHV1833 | PU/PD | 1 | ||
| gpio1_0
sys_nirq2 |
14 | I | |||||||||||
| Driver off | 15 | I | |||||||||||
| AB10 | Wakeup3 | sys_nirq1 | 1 | I | 15 | 1.8/3.3 | vdda33v_usb1 | Yes | IHHV1833 | PU/PD | |||
| gpio1_3
dcan2_rx |
14 | I | |||||||||||
| Driver off | 15 | I | |||||||||||
| Y12 | xi_osc0 | xi_osc0 | 0 | I | 1.8 | vdda_osc | No | LVCMOS Analog | |||||
| AC11 | xi_osc1 | xi_osc1 | 0 | I | 1.8 | vdda_osc | No | LVCMOS Analog | |||||
| AB12 | xo_osc0 | xo_osc0 | 0 | O | 1.8 | vdda_osc | No | LVCMOS Analog | |||||
| AA11 | xo_osc1 | xo_osc1 | 0 | A | 1.8 | vdda_osc | No | LVCMOS Analog | |||||
| J25 | xref_clk0 | xref_clk0 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp2_axr8 | 1 | IO | 0 | ||||||||||
| mcasp1_axr4 | 2 | IO | 0 | ||||||||||
| mcasp1_ahclkx | 3 | O | |||||||||||
| mcasp5_ahclkx | 4 | O | |||||||||||
| vin1a_d0 | 7 | I | 0 | ||||||||||
| clkout2 | 9 | O | |||||||||||
| timer13 | 10 | IO | |||||||||||
| gpio6_17 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| J24 | xref_clk1 | xref_clk1 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp2_axr9 | 1 | IO | 0 | ||||||||||
| mcasp1_axr5 | 2 | IO | 0 | ||||||||||
| mcasp2_ahclkx | 3 | O | |||||||||||
| mcasp6_ahclkx | 4 | O | |||||||||||
| vin1a_clk0 | 7 | I | 0 | ||||||||||
| timer14 | 10 | IO | |||||||||||
| gpio6_18 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H24 | xref_clk2 | xref_clk2 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp2_axr10 | 1 | IO | 0 | ||||||||||
| mcasp1_axr6 | 2 | IO | 0 | ||||||||||
| mcasp3_ahclkx | 3 | O | |||||||||||
| mcasp7_ahclkx | 4 | O | |||||||||||
| timer15 | 10 | IO | |||||||||||
| gpio6_19 | 14 | IO | |||||||||||
| Driver off | 15 | I | |||||||||||
| H25 | xref_clk3 | xref_clk3 | 0 | I | PD | PD | 15 | 1.8/3.3 | vddshv3 | Yes | Dual Voltage LVCMOS | PU/PD | |
| mcasp2_axr11 | 1 | IO | 0 | ||||||||||
| mcasp1_axr7 | 2 | IO | 0 | ||||||||||
| mcasp4_ahclkx | 3 | O | |||||||||||
| mcasp8_ahclkx | 4 | O | |||||||||||
| clkout3 | 9 | O | |||||||||||
| timer16 | 10 | IO | |||||||||||
| gpio6_20 | 14 | IO | |||||||||||
| Driver off | 15 | I |