SWRU626 December 2025 CC3501E , CC3551E
Quick Command is a simple, compact SMBus protocol that sends an address and 1-bit of data in the DIR bit of the I2C header byte to communicate a command to the Target, typically a "turn off" or "turn on". The I2C Controller peripheral has the ability to send a Quick Command by writing the target address and DIR value into the CSA register followed by a write to the CCTR register with a value of 0x07 such that the MBLEN bit field is set to 0. The Target logic also has quick command support built in.