SWRU626 December 2025 CC3501E , CC3551E
Flags in the SDMMC show status of communication with the card:
Error conditions generate interrupts. See Table 20-9 and register description for more details.
| Error hold in the SD_STAT Register | CC | TC | Comments | |
|---|---|---|---|---|
| 29 | BADA | No dependency with CC or TC. BADA is related to the register accesses. Its assertion is not dependent of the ongoing transfer. | ||
| 28 | CERR | 1 | CC is set upon CERR. | |
| 22 | DEB | 1 | TC is set upon DEB. | |
| 21 | DCRC | 1 | TC is set upon DCRC. | |
| 20 | DTO | DTO and TC are mutually exclusive.DCRC and DEB cannot occur with DTO | ||
| 19 | CIE | 1 | CC is set upon CIE. | |
| 18 | CEB | 1 | CC is set upon CEB. | |
| 17 | CCRC | 1 | CC can be set upon CCRC - See CTO comment | |
| 16 | CTO | CTO and CC are mutually exclusive. CIE, CEB and CERR cannot occur with CTO. CTO can occur at the same time as CCRC it indicates a command abort due to a contention on CMD line. In this case no CC appears. | ||
SD_STAT[21] DCRC event can be asserted in the following conditions: