SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
The processor core and the Nested Vectored Interrupt Controller (NVIC) together prioritize and handle all exceptions.
When handling exceptions:
All exceptions are handled in Handler mode.
Processor state is automatically stored to the stack on an exception, and automatically restored from the stack at the end of the Interrupt Service Routine (ISR).
The vector is fetched in parallel to the state saving, enabling efficient interrupt entry. The processor supports tail-chaining that enables back-to-back interrupts without the overhead of state saving and restoration.
Software can configure the priorities of these interrupts.
Exceptions can be specified as either Secure or Nonsecure. When an exception is taken, the processor switches to the associated security state. The priority of Secure and Non-secure exceptions can be programmed independently. It is possible to deprioritize Nonsecure configurable exceptions using the AIRCR.PRIS bit field to enable Secure interrupts to take priority.
When taking and returning from an exception, the register state is always stored using the stack pointer associated with the background security state. When taking a Non-secure exception from Secure state, all the register state is stacked, and then registers are cleared to prevent Secure data being available to the Non-secure handler. The vector base address is banked between Secure and Non-secure state. VTOR_S contains the Secure vector base address, and VTOR_NS contains the Non-secure vector base address. These registers can be programmed by software, and also initialized at reset by the system.
Vector table entries are compatible with interworking between Arm® and Thumb instructions. This causes bit[0] of the vector value to load into the Execution Program Status Register (EPSR) T-bit on exception entry. All populated vectors in the vector table entries must have bit[0] set. Creating a table entry with bit[0] clear generates an INVSTATE fault on the first instruction of the handler corresponding to this vector.