SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
The following cryptographic functions using energy-efficient accelerators and RNG functions are accelerated by the HSM:
Key Agreement Schemes
Elliptic Curve Diffie-Hellman with static or ephemeral keys (ECDH and ECDHE)
Elliptic Curve Password Authenticated Key Exchange by Juggling (ECJ-PAKE) (See Note below)
Diffie Hellman with static or ephemeral keys (DH, and DHE)
Key Derivation Methods:
Random (from DRBG)
SHA2 HMAC PRF (Pseudorandom Function)
AES CMAC PRF
Signature Processing
Elliptic Curve Diffie-Hellman Digital Signature Algorithm (ECDSA)
Edwards-curve Digital Signature Algorithm (EdDSA)
RSA PKCS #1 v1.5
RSA PSS
Message Authentication Codes
AES CBC-MAC
AES CMAC
HMAC with SHA2-224, SHA2-256, SHA2-384, and SHA2-512
Block Cipher Modes of Operation
AES CCM and AES CCM* (CCM-Star)
AES GCM
AES ECB
AES CBC
AES CTR
Hash Algorithms
SHA2-224
SHA2-256
SHA2-384
SHA2-512
Random Number Generation:
NIST SP800-90B compliant TRNG (True Random Number Generator)
AES-CTR DRBG (Deterministic Random Bit Generator)
Cryptographic key sizes and types include:
Advanced Encryption Standard (AES) key sizes of 128, 192, and 256 bits
RSA key sizes up to 3072 bits (Sign and Verify supported), and up to 4096 bits (Verify only)
Diffie-Hellman key sizes of 2048 bits and 3072 bits
Elliptic Curve Support
Short Weierstrass
NIST-P224 (secp224r1), NIST-P256 (secp256r1), NIST-P384 (secp384r1), NIST-P521 (secp521r1)
Brainpool-256R1, Brainpool-384R1, Brainpool-512R1
Montgomery
Curve25519
Twisted Edwards form, such as:
Ed25519
DPA countermeasures are implemented for:
AES operations
ECDH operations involving private key material
ECDSA
The HSM executes the HSM firmware from a secured flash region. The HSM firmware is verified by the HSM ROM before the HSM processor starts executing it. Secure firmware update of the HSM firmware image on-chip is supported by the system ROM bootcode and the HSM ROM.
The HSM also has its own data RAM region that is not accessible to the rest of the system (system CPU, DMA, debug access, and so on). The data RAM region is retained in low-power modes, supporting quick power-up of the HSM and retention of key material. In addition to the storage of key material in data RAM, the HSM supports importing and exporting wrapped key material (NIST SP800-38F) with a key unique to the device, known as a HW Unique Key (HUK). This allows the wrapped keys to be securely stored anywhere in the system’s nonvolatile (Flash) memory.
The HSM is accessible to the application running on the system CPU in a controlled manner via the HSM mailbox interface. The HSM is a bus controller in the device and can access the system memory directly, enabling better efficiency for moving data in and out during cryptographic operations.
The SimpleLink™ CC27xx software development kit (SDK) includes the encrypted and signed HSM firmware needed to be programmed on-chip for the HSM operation and drivers for all HSM functions. The SDK includes both SimpleLink™ APIs and Platform Security Architecture (PSA) APIs to enable easy use of the HSM features.
The algorithm is implemented on the application core using low-level HSM public key accelerator commands for acceleration.